全 387 件が検索されました。(341 - 360件を表示)

  • マニュアル

    ...00 E St IN CY 15 00 15 E IN 00 St CY TABLE COMPARE (@)TCMP(85) Compares a 4-digit hexadecimal value (CD) with values in table consisting of 16 words (TB: is the first word of the comparison table). If the value of CD falls within any of the comparison ranges, corresponding bits in result word (R) are set (1 for agreement, and 0 for disagreement). The table must be entirely within the one data area. TCMP(85) CD ...

  • マニュアル

    ...0 0 0 0 0 0 0 0 TABLE COMPARE – TCMP(85) Operand Data Areas CD: Compare data Ladder Symbols IR, SR, AR, DM, HR, TC, LR, # TCMP(85) @TCMP(85) CD CD TB TB R R TB: First comparison table word Description Flags IR, SR, DM, HR, TC, LR R: Result word IR, AR, DM, HR, TC, LR When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of ...

  • マニュアル

    ...ANO口 …一 0剖21 ou丁 0500 聖遷一灘 P『『m摺;nExm! {聾野討a藷el・Ser把sCirc=』藷 TO[)rOgra汀毒al)ara‖el.SerieSCi『CUR,Simp]y{)rOgramtheparal}eiCirC題tb拍CiくS lirst,andthen鮪ese酋esC;rCLsltb{O己ks.{n語efoliowin目exampie,fi『stprogram biocka、重henblockb. ロ メ H eco2soo3 200 トー義『、〔 02ζ}o A討絶ss 把s廿鑓tlon Da拍 oo。 oiLD… 0000 o。 出iA随 0001 OOO2 OR 0200 ooo3AND OOO2...

  • マニュアル

    ... they become apparent only after wiring” to “Run-away motors ... become apparent only after switching power on.” Connection point corrected at lower right of diagram on p.17. Corrected connection to IO213-8 of C100H-CPU01-E and removed incorrect ground connection from R88D-V10 ...

  • マニュアル

    ...0 0 0 0 0 0 0 0 TABLE COMPARE – TCMP(85) Operand Data Areas CD: Compare data Ladder Symbols IR, SR, AR, DM, HR, TC, LR, # TCMP(85) @TCMP(85) CD CD TB TB R R TB: First comparison table word IR, SR, DM, HR, TC, LR R: Result word IR, AR, DM, HR, TC, LR Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of ...

  • マニュアル

    .../Fax:35-1-1-941-7899 SPAIN OMRONELECTRONICSS.A. clArturoS◎ria95199,E-28027Madrid Tet:(91)4070211/Fax:(91)4070883 Tlx:491900MRESE 136 SWED副 OMRON∈LECTRONICSA.B. MusseronvagenIC,P.O.B◎x1223,S-14125Huddinge Td:{08)746004◎Fax:(08)7743095/...

  • マニュアル

    ...Indirectly addressed DM channel is non-existent. (DM data is not in BCD, or the DM area has been exceeded.) 4-7-4 Table Compare TCMP<85> TCMP<68> compares a four-digit hexadecimal value (CD) with values in a table consisting of 16 channels (...

  • マニュアル

    ....DiagnosticTableRead"fromtheReadNode'sStatusmenu. 一ー−No. −ltem Process NormaUError Remarks 1 τbtalSends Transmit 一一一 −Showsthgtotalcountoftransmissions(thetotalof詑ems2,10,12,13,14,16,andalhransmissionerrorsmth◆protocoltable}. 2 NormalSends Transm忙 Normal 一.-Showsthetotalcountofsuccessfuはransmissions、 3 ...

  • マニュアル

    ...2ク3_ RUN MONITOR DEBUG PROGRAM No No No OK 1.DisplaytheRackforwhichallocationsaretobechanged 2.PresstheFIKey.Thefunctionkeymenuwillchange. 一蹴■■■■■腫■國薩■國 Nbt嚥de⑭TNNE…T27 CX:SIα」CPuS…OUSIotnO12345678910 U川こUUnit=1tbrd㎜晒eagSlac2}...

  • マニュアル

    ...222 ---------------------[End of Page 9252]--------------------- } PCSetu Section7・2 Lgttgr D E F G H 1 J K L M Name Funcuon NormalaPP目cation(s) Startuppr㏄essing 1bspec廿ywhθtherthθuser Tb前abbusingaROMMemory programisloadedfromthe Cardwithoutabackupbattery。 MemoryCardwhenpoweris turnedon. 1/Orefresh τbsettherefreshmethodtocyclic, Tbreducethgcycletimebyushg zero.cross,orscheduled. imrnediatgrefreshingortoreduc6 surgevoltagesforACoutputs. Execution Detedlowbatte「y τbspec廿ydetectionofCPUbattery W)disablgdetectionwhgnbatteries controIS1 errors. arenotbeingused. (Execute Erroronpowero什 Tbspec目yifmomentaryp◎wer Tbgenθratθanerrorformomentary controiη intgrruptbnsaretobθtreatedas powerinterruptswhθnthgy errors. adverselyaffedsystemoperatbn. CPUstandby W〕specifywhethertheCPUlstogoonstandbyorstartoperatbnwhib i耐alizingthesystemordet㏄tingterminatorsinSYSMACBUS佗 Systems. MeasureCPUBus Tbspec話ywhetherornottheCPUBusUnitservicingcycleistobe Unit(CPUSIOU)cycle measured. Execution Executeprocess 取〕specifywhetherPeriphgral τbincrθasθprocessingcapacity controls2 Devicesaretobeserviced (speed)byusingasynchronous synchronouslyorasynchrronously ,pr◎ceSSlng・ w...

  • マニュアル

    ...: ExamPle: ProgramSamPle: StaternentSpec椚estheDATAstatementtobereadbysubsequentREAD statements, RESTORE{{"ηθ−no.1ηabθ{}】 SubsequentREADstatementswi‖readdatafromtheDATAstatementatthe specified〃ηθ一ηo.or爵'abeL lf〃ηe−ηo.or/abθljsomitted,thefirstDATAstatementinthetaSkisselected, NoteOthertask'sDATAstatementscannotbespecifiedforreadjng. RESTORE700 10'testco㎜andname:RESTORE 20PARACTO 30Dl二MA$(10)...

  • マニュアル

    ...ト AOO115 READ − 曲 ㌔声 → E →一一:寸ε↓lflー」}・ーN 工 L F … 32KW 4.WhenENTispressedagain,thesearchbeginsagainfromaddressOOOOO andthecursorstopsatthefirstinstructionblockcontainingaconditionwith AOO115. 一ドH FindingMOV(030)withthe FunctionCode ...

  • マニュアル

    ...0 0 0 0 0 0 5-16-5 TABLE COMPARE – TCMP(85) Operand Data Areas CD: Compare data Ladder Symbols IR, SR, AR, DM, HR, TC, LR, # TCMP(85) @TCMP(85) CD CD TB TB R R TB: First comparison table word IR, SR, DM, HR, TC, LR R: Result word IR, AR, DM, HR, TC, LR Description When the execution condition is OFF, TCMP(85) is not executed. When the execution condition is ON, TCMP(85) compares CD to the content of ...

  • マニュアル

    ... 231. 50 Section 1-5 CQM1 Interrupt Functions Controlling High-speed Counter 0 Interrupts 1,2,3... 1. Use the CTBL(63) instruction to save the comparison table in the CQM1 and begin comparisons. (@)CTBL(63) P C ...

  • マニュアル

    ...0 0 0 0 0 0 5-17-5 TABLE COMPARE – TCMP(85) Operand Data Areas CD: Compare data Ladder Symbols IR, SR, AR, DM, HR, TC, LR, # TCMP(85) @TCMP(85) CD CD TB TB R R TB: First comparison table word IR, AR, DM, HR, TC, LR R: Result word IR, SR, AR, DM, HR, TC, LR Limitations ...

  • マニュアル

    ...DO50150100 蔦mperaturgController2 DO50230000 DO50240020 DO50250100 TbmperatureController3 DO50330000 DO50340030 DO50350100 1bmperatureContro‖er4 DO50430000 DO50440040 DO50450100 1bmperatureControlbr5 DO50530000 DO50540050 DO50550100 DownloadData2 NoteUpPervalue:bitaddress Lowervalue:data 脆mperatumController Sθtpoint(勺htmostbit) Setpoht{leftmostbit) ...

  • マニュアル

    ... of the high-speed counter is maintained in SR 230 and SR 231. Controlling High-speed Counter Interrupts 1, 2, 3... 1. Use the CTBL(––) instruction to save the comparison table in the ID Controller and begin comparisons. (@)CTBL 000 C ...

  • マニュアル

    ...1.Removethecomectorcover、 Thecoverthathasbeenremovedcanbeattachedtothe backoftheUnitforc◎nvenience, tokeepitfromgettinglost。 一働 Cover Useasmallstandard screwdriverorsimilar objecttoopenthecover,・宝ヨ 2.lnsertthecableconnectorintotheTeachingBox. グ Makesurethattheconnectoris facing旧theproperdirection, andthensnapjtintoplace. 74 ---------------------[End of Page 2927]--------------------- ConnectintheTeachinBox Section8・3 3.lnserttheothercableconnectorintotheMCUnitconnectormarked"...

  • マニュアル

    ...7,2,3..。 UsethefollowingproceduretoconneCttheTeachingBoxtotheMCUnit. 1.Removetheconnectorcover. Attachtheremovedo◎ve「t◎ therearsurfacgnottoloseit. Openthe。 。 verusinga smati-sizeflat-blade screw. 2 ⊇ '.一、、 一 ○[=ol ◎ lCoverattached 1 2.P.iugtheConnectingCableintotheconnector. theconnectorandpushitinuntil aradick. 3.PlugtheConnectingCableintotheMCUn詑connectormarked"...

  • マニュアル

    ...there are two Masters set to “scan list disabled mode” in the network. Note 1. The CompoBus/D Configurator is needed to allocate I/O. 2. When the Masters (A and B) form separate networks with communication cycle times of TA and ...