全 391 件が検索されました。(281 - 300件を表示)

  • マニュアル

    ... result. When the input data is a value between the upper limit data and lower limit data, the value of the input data is returned as the result. The same data type must be set for the arguments and the return value. Result Upper limit: ...

  • マニュアル

    ... or Servo manuals carefully and be sure you understand the information provided before setting up or using an application for a drive. Drive type Inverters Servomotors/ Servo Drives Manual Name SYSDRIVE JX Series Models 3G3JX Compact Simplified Inverters User's Manual SYSDRIVE ...

  • マニュアル

    ... be sure you understand the information provided before setting up or using an application for a drive. Drive type Inverters Manual Name SYSDRIVE JX Series Models 3G3JX Compact Simplified Inverters User's Manual Cat. No. (suffixes omitted) I558-E1 SYSDRIVE ...

  • マニュアル

    ...#0/Ch1_RdAI Conversion Data Contents Indicates the input 1 A/D conversion value. z Program Example P_On EN MinLimit J01_Ch1_RdAI MaxLimit A-2-2 OverUnderLimit ZoneCmp Out MN In MX Upper and Lower-limit Alarm (with Standby Sequence) z Outline Comparisons are made to the upper and lower limits of the A/D conversion values or D/A output values after the value falls within the range between the upper limit and lower limit following the beginning of operation. If they fall outside the specified range, the Alarm Flag will turn ON. In this example, ...

  • マニュアル

    ....Kp:=1; PIDFFOpr.Ki:=2; END_IF; // Power ON IF _EC_PDSlavTbl[SlaveNode] THEN MCP1Enable:=TRUE; ELSE MCP1Enable:=FALSE; END_IF; //DeadBand between 0.0 and 0.1. BandedPos:=\\OmronLib\MC_Toolbox\DeadBand(MN:=DeadBandLow,In:=MC_Axis001.Act.Pos,...

  • マニュアル

    ... distance to the travel distance of each axis controlling the stage by using reverse kinematics calculation (CalcInverseKinematics FUN). 4 - 46 Sysmac Library User's Manual for Visual Feedback Alignment Library (W608) 4 Individual Specifications of FB/FUN • Diagram of converted image Y axis (...

  • マニュアル

    ...Settings SENSING FILTER OUTPUT HOLD 0RESET Default Value Option/Range Pages SEL CH - Input A to input I CALC CH OFF, CH (input A to input I), CALC p.3-15 (THICK, STEP, K+mX+nY, AVE, MAX-MIN) SMOOTH ON OFF, ON AVERAGE 1 1, 2, 4, 8, 16, 32, 64, 128, 256, 512, 1024, 2048, 4096 DIFF OFF OFF, ON - SCALING OFF OFF, ON (AUTO, MAN) - TYPE OFF OFF, PEAK, BOTTOM, P-P, AVERAGE, SAMPLE TRIGGER EXT EXT, SELF-UP, SELF-DN - DELAY OFF OFF, ON (T-DELAY, T-TIME) - TYPE REAL REAL, HOLD - OFFSET 0 -999.99 ...

  • マニュアル

    ...% 5: 62.5% 6: 75% 7: 87.5% 0: OFF 1: ON 0: Timing A 1: Timing B 1 to 5 0: OFF 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX;+nY ZS Series CompoWay/F Communication Command Reference When the measurement object is changed, the settings are initialized according to the selected object. TASK1 settings. The settings in Unit Number 28h are valid only for multi-task mode. Section 3 Setting Value Obtaining and Changing Command Parameter Parameter X 28h 4h Parameter Y 5h Parameter K 8h Parameter M -100 to 100 (1div:...

  • マニュアル

    ... of Parameters (ZS-HLDC) Unit No. 40 Data No. 0 Parameter Measurement mode Setting range/Output range 0: OFF Others TASK1 settings. 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX; +nY 3 Parameter X 0: None 1: TASK 1 2: TASK 2 3: TASK 3 4: TASK 4 4 Parameter Y 0: None 1: TASK 1 2: TASK 2 3: TASK 3 4: TASK 4 5 Parameter K -999999999 to 999999999 (nm) 8 Parameter M -100 to 100 (1div: 0.1) 9 Parameter N -100 to 100 (1div: 0.1) 1 Surface for measurement (...

  • マニュアル

    ...OBJECT ([THICK] is not displayed.) – SYNC (Same as Single-Task mode) – TASKSET NONE*, p.5-24 SETTING LASER MEASURE TASK2 to 4 18 ZS-HL User’s Manual AVERAGE, PEAK, BOTTOM, THICK, STEP, K+mX+nY FILTER (Same as Single-Task mode) – OUTPUT (Same as Single-Task mode) – TASKSET p.5-24 MEASURE NONE*, AVERAGE, PEAK, BOTTOM, THICK, STEP, K+...

  • マニュアル

    ...Set any equation to perform addition/subtraction on the measurement result. The equation can be substituted with measurement results obtained by other tasks. Also, when using two Controllers in a gang-mount configuration, calculations can also be performed across channels. Allowable equation: K+...

  • マニュアル

    ...This is the X coordinate of the measured edge 1 position. -99,999.9999 to 99,999.9999 Y1 Edge 1 position Y This is the Y coordinate of the measured edge 1 position. -99,999.9999 to 99,999.9999 MX Midpoint X This is the X coordinate of the -99,999.9999 to 99,999.999 measured edge midpoint position. MY Midpoint Y This is the Y coordinate of the -99,999.9999 to 99,999.999 measured edge midpoint position. SX0 Edge0 ref. position X This is the X coordinate of the (edge 0 reference position X) ...

  • マニュアル

    ... For the setting of measurement area to control of light adjustment, refer to the following: Setting Light Exposure Time Control Mode p.129 Setting Exposure Time Control Mode p.232 Performing Calculations Perform calculations using the results calculated by the tasks. The calculation formula is ...

  • マニュアル

    ...-KR V780-HMD68-ETN-CN V780-HMD68-ETN-TW V780-HMD68-ETN-IN V780-HMD68-ETN-ID V780-HMD68-ETN-MY V780-HMD68-ETN-SG V780-HMD68-ETN-EU V780-HMD68-ETN-RU V780-HMD68-ETN-US V780-HMD68-ETN-MX Slave Reader/Writer V780-HMD68-ETN-JP-S V780-HMD68-ETN-KR-S V780-HMD68-ETN-CN-S V780-HMD68-ETN-TW-S V780-HMD68-ETN-IN-S V780-HMD68-ETN-ID-S V780-HMD68-ETN-MY-S V780-HMD68-ETN-SG-S V780-HMD68-ETN-EU-S V780-HMD68-ETN-RU-S V780-HMD68-ETN-US-S...

  • マニュアル

    ...-KR V780-HMD68-EIP-CN V780-HMD68-EIP-TW V780-HMD68-EIP-IN V780-HMD68-EIP-ID V780-HMD68-EIP-MY V780-HMD68-EIP-SG V780-HMD68-EIP-EU V780-HMD68-EIP-RU V780-HMD68-EIP-US V780-HMD68-EIP-MX Slave Reader/Writer V780-HMD68-ETN-JP-S V780-HMD68-ETN-KR-S V780-HMD68-ETN-CN-S V780-HMD68-ETN-TW-S V780-HMD68-ETN-IN-S V780-HMD68-ETN-ID-S V780-HMD68-ETN-MY-S V780-HMD68-ETN-SG-S V780-HMD68-ETN-EU-S V780-HMD68-ETN-RU-S V780-HMD68-ETN-US-S...

  • マニュアル

    ...-Task mode) – SETTING LASER MEASURE TASK2 to 4 18 ZS-HL-N User’s Manual OBJECT ([THICK] is not displayed.) – SYNC (Same as Single-Task mode) – TASKSET NONE*, AVERAGE, PEAK, BOTTOM, THICK, STEP, K+mX+nY p.5-24 FILTER (Same as Single-Task mode) – OUTPUT (Same as Single-Task mode) – TASKSET p.5-24 MEASURE NONE*, AVERAGE, PEAK, BOTTOM, THICK, STEP, K+...

  • マニュアル

    ...% 5: 62.5% 6: 75% 7: 87.5% 0: OFF 1: ON 0: Timing A 1: Timing B 1 to 5 0: OFF 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX;+nY ZS-HL-N Series CompoWay/F Communication Command Reference When the measurement object is changed, the settings are initialized according to the selected object. TASK1 settings. The settings in Unit Number 28h are valid only for multi-task mode. Section 3 Setting Value Obtaining and Changing Command Data No. 3h Parameter Parameter X 28h 4h Parameter Y 5h Parameter K Setting range/...

  • マニュアル

    ...prevention timing 1: Timing B 1 to 5 5 0 Gain setting 40 0 Measurement mode 0: OFF Others TASK1 settings. 1: Average 2: Peak 3: Bottom 4: Thickness 5: Gap 6: K+mX; +nY 3 Parameter X 0: None 1: TASK 1 2: TASK 2 3: TASK 3 4: TASK 4 4 Parameter Y 0: None 1: TASK 1 2: TASK 2 3: TASK 3 4: TASK 4 5 Parameter K 8 Parameter M -999999999 to 999999999 (nm) -100 to 100 (1div: 0.1) 9 Parameter N -100 to 100 (1div: 0.1) 1 Surface for measurement (Area 1)...

  • ...術相談 メキシコ国内フリー通話 : 01 - 800 - 226 - 6766 TEL / FAX FAX : 52 - 55 - 5901 - 4300 対応言語 スペイン語、英語、日本語 Web site https://industrial.omron.mx 営業所所在地 Monterrey TEL : 52-81-1156-9910 FAX : 52-81-1086-2020 ジャパンデスクメキシコ TEL : 52-47-2723-8900 (内線 8995) BRAZIL ブラジル 住所 OMRON ELETRONICA DO BRASIL LTDA. Alameda Vicente Pinzón, 51 - 3 º andar, Vila ...

  • ...OMRON ELECTRONICS DE MEXICO Lamartine 238, 4th floor, Col. Chapultepec Morales, Mexico Df, Zip 11570, Mexico TEL : 52-55-5901-4300 / Technical Consultation Toll-free within Mexico : 01-800-226-6766 FAX : 52-55-5901-4300 Spanish, English, and Japanese https://industrial.omron....