全 530 件が検索されました。(261 - 280件を表示)
- マニュアル
... type out of range 16#0000 0004 Trapezoid area data monitoring lower limit elapsed time out of range The value of TrapezoidData.AlarmType (Alarm Type) is outside of the valid range. The value of TrapezoidData.MonitorLowerTi ...
- マニュアル
... is the target of calculation. Valid range Depends on data type. ARRAY [0..15] OF BOOL Depends on data type. FALSE ARRAY [0..15] OF DINT Depends on data type. 0 OmronLib\DIM_Me asurement\sThres holdParams ― ― BOOL Depends on data type. FALSE BOOL Depends on data type. FALSE FALSE: The sensor input value with the array element number set to FALSE is not the target of calculation. Input Input Value Threshold*1 Threshold Specify one or more sensors. The input value obtained from a measurement sensor. The measurement values of the sensors are input for each array element....
- マニュアル
... network drive • The local drive in drive bay B, when installed. NY-series NYB/NYP Industrial PC Operating Systems and Software Utilities Manual (W616) 7-11 7 Maintenance 7 8 9 Select Next. The following window will appear: Select Let ...
- マニュアル
... network. Additional Information Preferred locations for an automatic backup are: • A network drive • The local drive in drive bay B, when installed. 7-4 NY-series NYE Industrial PC Operating Systems and Software Utilities Manual (W635) 7 Maintenance 7 Select Let ...
- マニュアル
.../NYP Industrial PC Security Guidelines User's Manual (W661) 3-1 Windows Security Functions and Configuration Create a Custom Backup with Windows Backup 3-25 3 Security Functions 7 8 9 Select Next. The following window will appear: Select Let ...
- マニュアル
...Make sure that you are logged onto the computer as a user with administrator rights. ● STEP2 If the right dialog box is displayed, select the Don't search online Option. ● STEP3 Select the following: I don't have the disc. Show ...
- マニュアル
... Card ■ Inserting the Memory Card 1. Press the EJECT button on the Memory Card Dummy card EJECT button 2. Insert the Memory Card. Insert the Memory Card with its label surface facing up. Com pact Flas h ...
- マニュアル
...When the following window is displayed, select Locate and install driver software (recommended) Button. 52 RFID System User’s Manual SECTION 2 Installation, Connections, and Wiring 4. When the following window is displayed, select I don’t have the disc. Show ...
- マニュアル
... Measurement Mode 42 44 Setting Thresholds - T Mode 45 Functions and Operations during Operation RUN Mode 46 Switching the Measured Value Display Executing and Canceling a Zero Reset 46 47 BASIC OPERATIONS S e t t i ng ...
- マニュアル
...A trigger signal is input to control measurement timing. ZG2-WDS70 ZG2-WDS22 ZG2-WDS8T ZG2-WDS3VT Controller Performs measurement processing and outputs the result. ZG2-WDC11/WDC41 Smart Monitor ZG2 (exclusive PC software) ...
- マニュアル
...2 Protective dummy card EJECT button 3 Press the EJECT button at the side of the Memory Card slot. Remove the protective dummy card from the unit. Insert the Memory Card. Com pact Flas h ME MO RY OM CA RD IN A RON Memory Card Removing Memory Cards Important Before removing a Memory Card from the unit, make sure that the CF power LED and access LED are both OFF. If a Memory Card is removed with these LEDs still ON, there is the possibility that data stored on the Memory Card might be lost or the Memory Card ...
- マニュアル
...Reader/Writer V780-HMD68-ETN- 24-VDC power supply RF Tag V780-A-JIME-Z3BLI-10*1 (recommended) Host device (e.g., PLC) Recommended Power Supply Cable: XS5F-D42-80-F (made by OMRON) Recommended Ethernet Cable: XS5W-T42-...
- マニュアル
... g Packing weight Approx. 174 g (including packing) Main body Dimension 44.5 (W) × 44.5 (D) × 25.4 (H) mm Packing Dimension 170 (W) × 117 (D) × 86 (H) mm Accessories Instruction manual ("Read me first"), Compliance Sheet (CE) LED class Risk Group Exempt (IEC 62471-1) Safety standards EN61326-1: 2013 FCC Part 15, Subpart B (Class A) KC CISPR 11, IEC 61000-4-2: 2008 UL60950-1 RCM, EAC, BSMI, BIS Material Case Aluminum diecast, alumite (black) Reading window Acrylic *1. These are the code types supported based on Omron’s read capability ...
- マニュアル
...Reader/Writer V780-HMD68-EIP- 24-VDC power supply RF Tag V780-A-JIME-Z3BLI-10*1 (recommended) Host device (e.g., PLC) Recommended Power Supply Cable: XS5F-D42-80-F (made by OMRON) Recommended Ethernet Cable: XS5W-T42-...
- マニュアル
... due to no workpiece measured, averaging in progress, etc. This indicates that the laser emission is OFF due to LD-OFF input, etc. The indicator status is unstable when a communications error occurs between the Sensor Head and the Amplifier Unit. Additional Information • The Find-...
- マニュアル
...: Command code 1 to 6: Data*1 *1. Refer to A-3-7 Amplifier Unit Operation Command Object (Class ID: 392 Hex) on page A-39 for details. Role Sends control commands to the Amplifier Unit (sampling period teaching, find-...
- マニュアル
... 0xFF (Bit control) Bit 0: Laser emission status (0: Emitting, 1: OFF) Bit 1: Zero reset status (0: Cancel, 1: Execute) Bit 2: Timing status (0: Non-sampling, 1: Sampling) Bit 3: Reset status (0: Not reset, 1: Resetting) Bit 4: Find-...
- マニュアル
...R +0 When the IO-Link device numbers specified in writing are out of range, an out-of-range error will be generated without switching. The readout will return the current port numbers. - l RW +0 0: Cancel a Find ...
- マニュアル
...Meaning Source 00085 Cause 00087 Reserved Event code R/W Reserved *2. Reserved Event code R 00083 00088 Reserved Event code 00081 00086 Event 0 occurred Event 4 Find Me 00082 Event 1 occurred Event 3 Clear the latest event*2 00080 Event 4 occurred Event code Source Event 2 Re ser ve d Event 5 occurred Event 0 Cause Details available Meaning of event 0 Event 2 occurred 00078 0 Clear the latest error*2 Event 1 1 3 Count 00077 2 Sub-index number that caused the latest error Reserved Type of event 0 Event 0 3 Latest ...
- マニュアル
...When the IO-Link device numbers specified in writing are out of range, an out-of-range error will be generated without switching. The readout will return the current port numbers. --- l 00065 10A h 0 (This product) Find ...