全 270 件が検索されました。(241 - 260件を表示)

  • マニュアル

    ...Use an SELV power supply with overcurrent protection. An SELV power supply has redundant or reinforced insulation between the I/ O, an output voltage of 30 Vr.m.s and a 42.4-V peak or maximum of 60 VDC. We recommend these Power Supplies. • ...

  • マニュアル

    ... noise immunity, ground at less than 100 Ω. For a ground cable, use a cable of 2 mm2 diameter minimum (green cable), and keep the cable length to within 20 m. Recommended Power Supply (Small, DIN Rail Type) Model Output Input voltage ...

  • マニュアル

    ... shown in the following diagram. Details are provided later in this section. ! Caution Turn OFF the power to the Controller before connecting or disconnecting cables. Connecting or disconnecting cables with power turned ON can damage peripheral devices. Power Supply → p. 12 (OMRON’s ...

  • マニュアル

    ... shown in the following diagram. Details are provided later in this section. ! Caution Turn OFF the power to the Controller before connecting or disconnecting cables. Connecting or disconnecting cables with power turned ON can damage peripheral devices. Power Supply → p. 8 (OMRON’s ...

  • マニュアル

    ... as shown in the following diagram. Details are provided later in this section. ! Caution Turn OFF the power to the Controller before connecting or disconnecting cables. Connecting or disconnecting cables with power turned ON can damage peripheral devices. Power Supply → p.14. (OMRON’s ...

  • マニュアル

    ... the video monitor. K Connects to the Console. 8 Section 2-2 Connections 2-2 Connections Connect the basic component as shown in the following diagram. Details are provided later in this section. Power Supply → p. 10 (OMRON’s ...

  • マニュアル

    ... to the monitor. K Connects to the Console. 8 Section 2-2 Connections 2-2 Connections Connect the basic component as shown in the following diagram. Details are provided later in this section. Power Supply → p. 10 (OMRON’s ...

  • マニュアル

    ... the Two-camera Unit as well as the power to the F150 itself before connecting or disconnecting cables. 12 Z141-E1-03.book Page 13 Monday, July 24, 2006 5:16 PM Section 2-3 Connections Power Supply → p. 14 (OMRON's ...

  • マニュアル

    ...RUN ERROR OR BUSY GATE DO15 CONSOLE COMOUT *Camera Cable F150-VS (3 m) CAMERA0 RS-232C/422 PARALLEL Power Supply CAMERA1 MONITOR page 18 + 24VDC − Recommended model: OMRON S82K-05024 Monitor Cable F150-VM (2 m) BNC Jack (Included with the F150-VM.) Monitors Color LCD Monitor (F150-M05L) Monochrome CRT Video Monitor(F150-M09) POWER SYNC (RCA plug input) 8 (BNC input) The Monitor is used to check the image and display menus when making settings. Section 2-1 Basic System Configuration Cameras Images of measurement objects are obtained using Cameras. Up to 2 Cameras can be connected ...

  • マニュアル

    ...Applicable Wire Type Japan Solderless Terminal 1.25-N3A AWG24 to AWG16 Fork Japan Solderless Terminal 1.25-Y3A (For M3) ♦ Recommendable DC power supply (small-sized) (OMRON) Model Output Capacity Input Voltage ...

  • マニュアル

    ... connector of host as shown below. RS-232C Connecting Cable (V690-A4@) IBM PC/AT or compatible V690-HMG01A Antenna Ground to 100 Ω or less Switch, etc. 24 VDC power supply • Recommended 24 DC Power Supply ...

  • マニュアル

    ... will not light and the OK indicator will be unstable for 30 seconds after power is turned ON. 9 Section 2-2 Connections 2-2 Connections Connect the basic components. Power supply “page 11 Recommended OMRON Power Supplies ...

  • マニュアル

    ...F150-A20 F150-S1A Use this Unit to connect two Cameras to a single V530-R150. (The Cameras shown on the left can be connected.) 14 Section 2-2 Connections Power Supply → page 16 (We recommend the OMRON ...

  • マニュアル

    ... OFF the download function. REFERENCE Refer to page 146 in the Operation Manual. 20 Z500 Setup Manual Z158-E1-02C.book Page 21 Wednesday, August 9, 2006 6:13 PM SECTION 1 Wiring and Connection Power Supply Recommended model: OMRON ...

  • マニュアル

    ..., the Z300 goes into Visual Mode when the power supply is turned ON. The DIP switch is factory-set to VISUAL. ∗Components marked with an asterisk are specially designed for the Z300. Other products cannot be used. Power Supply Recommended model: OMRON ...

  • マニュアル

    ... from table. 02 May 2005 Information on warranty and liability at the front of the manual updated. The following changes were also made. Pages 3 and 40: "Video monitor" changed to "monitor." Page 4: Information on securing the video monitor removed. Page 8: "...

  • マニュアル

    ...1.25-N3A J.S.T Mfg. Co., Ltd. 1.25-Y3A Applicable wire size AWG24 to 16 Shape Forked 6.5 mm max. (For M3 terminal) Recommended DC Power Supplies (Miniature, by OMRON) Note Model number S82K-03024 Output capacity 24 V DC, 1.3 A Input voltage 100/200 V AC S82J-0224 24 V DC, 1.1 A 100 V AC 1. Although adequate measures have been taken inside the I/O Sensor Unit for noise entering on the power supply line, supplying power through a line filter can be used to greatly attenuate ground noise. 2....

  • マニュアル

    ... (including the case of short-circuit), or – a secondary fuse or other such secondary circuit protective device used to limit the available current shall be rated at not more than a value 4.2 amperes (for the power supply voltage of 24VDC) Recommended power supply: ...

  • マニュアル

    ... connecting or disconnecting cables. The peripheral devices may Basic System Configuration be damaged if connected or disconnected while the power supply is turned on. * Console Z300-KP (2m cable) ESC TRIG ENT Power Supply Recommended model: OMRON ...

  • マニュアル

    ... connecting or disconnecting cables. The peripheral devices may Basic System Configuration be damaged if connected or disconnected while the power supply is turned on. * Console Z300-KP (2m cable) ESC TRIG ENT Power Supply Recommended model: OMRON ...