全 469 件が検索されました。(201 - 220件を表示)

  • マニュアル

    ...Host Link: CS/CJ-series PCs, C-series PCs, CVM1/CV-series PCs, SRM1 Can be connected to CPU Units, Host Link Units, and SRM1. However, connection is not possible to some models of CPU Unit and SRM1. NT Link: CS/CJ-series PCs, CPM1, CQM1, ...

  • マニュアル

    ... I/O data to event memory and read/write event memory. • Send/receive FINS messages to/from devices on the DeviceNet network (only for devices that support FINS). (Not all devices support FINS communications functions with Open Network Controllers (e.g., C200HX/HE/HG or ...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Reducing Response Time (C200H, C200HS, C200HX/HG/HE(-Z)) . . . . . . . . . . . . . . . . Programming Examples . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 7 Error Processing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7-1 7-2 7-3 SR Area Flags . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Examples . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Error Tables . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 8 Inspection and Maintenance . . . . . . . . . . . . . . . . . . . . . . . Appendix A Standard Models . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . B Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Glossary . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . vii About this Manual: A PC Link System enables use of the LR (Link Relay) data area as a common data area shared by all PCs in the PC Link System, thus simplifying programming, settings, and data exchange between PCs and permitting effective use of inputs and outputs. This manual has been written to provide the ...

  • マニュアル

    ...Data area 0 DM 1 IR 2 LR 3 HR 4 AR Note Use only the following words in the DM and IR areas: DM 0000 to DM 1999 and IR 000 to IR 235. Although the C200HS provides larger areas, if any words not within the specified ranges are used, an error will occur and an error code of 34 will be output. Number of Transfers Word n+3, bits 15 through 08 Set to between 1 and 3. When changing range parameters, data for up to three ranges can be transferred at the same time. When transferring the ...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Communications Protocol (C200HS/HX/HG/HE only) . . . . . . . . . . . . . . . . . . . . . . . . . . Frame Checksum (FCS) Calculation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 4 Commands and Responses . . . . . . . . . . . . . . . . . . . . . . . . 4-1 4-2 4-3 4-4 4-5 4-6 4-7 4-8 4-9 4-10 4-11 4-12 4-13 4-14 4-15 4-16 4-17 4-18 4-19 4-20 TEST . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . STATUS READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ERROR READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . IR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . HR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . AR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . LR AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . TC STATUS READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . DM AREA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . FM INDEX READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . FM DATA READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . PV READ . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SV READ 1 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SV READ 2 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SV READ 3 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . STATUS WRITE . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . IR ...

  • マニュアル

    ... Section: ASCII Unit Refresh timing Words n to n+2 OUT refresh Word n+3 IN refresh 4 words are used (n: 100 + 10 + unit no.) Transferred to each Unit every time the I/O data is refreshed. SYSMAC C200H, ...

  • マニュアル

    ... Node Bypass (optical systems only) functions prevent the network from failing when one Unit fails. The Internode Echo Test function aids in communications troubleshooting. Remote monitoring of the network’s operating status also aids in troubleshooting and quick correction of communications problems. Improvements on the ...

  • マニュアル

    ... Control Unit will not operate normally if the cycle time of the CPU Unit is less than 8 ms. • If the cycle time is less than 8 ms (e.g., the program execution time is short), increase it to at least 8 ms. • For the C200H, ...

  • マニュアル

    ... any static built-up. Not doing so may result in malfunction or damage. !Caution The cycle time of the CPU Unit must be a minimum of 20 ms. If the cycle time is too short, the PID Control Unit will not operate properly. • For C200H, ...

  • マニュアル

    ... Units) CVM1, CV Series CVM1-DRM21-V1 CPU or Expansion CPU Rack (Classified as CPU Bus Units) CS Series C200HW-DRM21-V1 CPU Rack or Expansion I/O Rack (Classified as Special C200HZ/HX/HG/HE I/O Units) ...

  • マニュアル

    ... with other CPU Units. EPROM Memory Cassette With an EPROM Memory Cassette, the program is written using a PROM Writer. The ROM is mounted to the Memory Casette and then installed in the CPU Unit. I/O data cannot be stored. Model Capacity ...

  • マニュアル

    ... is provided in the C200HX/HG/HE Programmable Controller Installation Guide. A table of other manuals that can be used in conjunction with this manual is provided in Section 1 Introduction. Provided in Section 2 Hardware Considerations is a description of the differences between the ...

  • マニュアル

    .... 295 viii About this Manual: This manual describes the installation and operation of the C200H-ASC11/ASC21/ASC31 ASCII Units and includes the sections described below. These ASCII Units can be used with the C200HX/HG/HE, ZE-version C200HX/HG/HE, C200H, ...

  • マニュアル

    ...Console External appearance Model WS02-CXPC@-EV@ CQM1-PRO01-E C200H-PRO27-E CVM1-PRS21-EV1 Note Applicable PLCs CS/CJ-series, C200HX/HG/HE, CVM1-series, and CQM1H-series PLCs C200HX/HG/HE, C200H/C200HS...

  • マニュアル

    .... . . . . . . . . . . . . . . . . . . 3 1 Section 1-1 Features 1-1 Features The C200H-CT021 High-speed Counter is a Special I/O Unit for the C200H, C200HS, C200HX, C200HG, and C200HE PCs. The High-speed Counter Unit has the following features. Two Built-in Counters The High-speed Counter Unit has two high-speed increment/decrement counters, each of which can be connected to an incremental encoder with open collector output to count line driver input pulses at a rate of 75,000 cps max. Built-in Line Driver Input Circuit An encoder with RS-422 line driver output can be ...

  • マニュアル

    ...500 grams or less (Connectors excluded) External dimensions 130.0 x 34.5 x 100.5 mm (H x W x D) Voltage g fluctuation tolerance Internal current consumption Specifications other than those shown above conform to those for the SYSMAC C200H/...

  • マニュアル

    ... known as the “PC data area interface.” Allocated Words The interface area varies with the type of the PC to which the MC Unit is mounted. Refer to the following examples. Refer to Section 6 PC Data Area Interface for more details. C200H/...

  • マニュアル

    ...peripheral port. (Use Host Link mode when connecting a PT through an RS-232C Adapter.) The RS-232C port on an SRM1-C02-V2 can be used to connect directly to an IBM PC/AT or compatible computer, OMRON PT, or PC (C200HX/HG/HE, ...

  • マニュアル

    ... be used with the SYSMAC-NCT Support Tool. Applicable Position Control Units Corresponding PCs C200HW-NC113/213/413 C200HX/HG/HE(-Z) PCs C500-NC113/211 C-series and CV-series PCs Note The SYSMAC-NCT Support Tool cannot be used with C200H/...

  • マニュアル

    ... operation of the C200H-AD003 Analog Input Unit, the C200H-DA003/DA004 Analog Output Unit, and the C200H-MAD01 Analog I/O Unit and includes the sections described below. The C200H-AD003 Analog Input Unit converts analog sensor output to digital format and transmits it to C200H, ...