全 1073 件が検索されました。(181 - 200件を表示)

  • マニュアル

    ... operation is stopped. (2) When the control cycle is short due to the 2-ms output resolution, the Unit may not operate as set. For example, when the Control Cycle = 1 s and the Output Minimum ON/OFF Duration = 0.1%, the calculation becomes 1 ...

  • マニュアル

    ... will stop. Press O + M Keys for at least 1 s Only when Manual Mode was used just before power OFF Operation in progress Power ON Press O Key for at least 1 s or S Key for at least 1 s*1 Level changes automatically. Press O + M Keys for at least 3 s.*2 Press the O Key once. Manual Control Level Used to set the MV manually. Operation Level Press O Key for at least 3 s while a-m is displayed.*2 Press S Key.*3 S Key for at least 1 ...

  • マニュアル

    ... set protection for operations. Starting in manual mode Power ON Press O and M Keys for at least 3 s.*2 Level changes automatically. Operation in progress Manual Control Level Press O or S Key for at least 1 ...

  • マニュアル

    ... After Power ON parameter is set to Manual in the Initial Setting Level Press O + M Keys for at least 1 s Operation in progress Power ON Press O Key for at least 1 s or S Key for at least 1 s*1 Level changes automatically. Press O + M Keys for at least 3 s.*2 Press the O Key once. Manual Control Level Used to set the MV manually. Operation Level Press O Key for at least 3 s while a-m is displayed.*2 Press S Key.*3 S Key for at least 1 ...

  • マニュアル

    ... when the Operation After Power ON parameter is set to Manual in the Initial Setting Level Used to set protection for operations. Power ON Operation in progress Press O Key for at least 1 s or S Key for at least 1 ...

  • マニュアル

    ...□) 回転低下検出(形AMD-SL□) 形H7CC-R11□ パラメータ totm (TOTM) 設定値 lolo (下限) hihi (上限) 計測範囲 0.01 ∼ 0.1s(形AMD-S□1) cnts 0.1 ∼ 1s(形AMD-S□2) (CNTS) 1 ∼ 10s(形AMD-S□3) 平均回数 無し avgn off (AVGN)(平均化処理なし) 固定 (0.1 ∼ 10s) stmr 0 .0 ∼ 9 9 . 9 (STMR) (0.0s)(99.9s) 起動補償 タイマ 入力モード ...

  • マニュアル

    ... for the command data to be transferred to the DeviceNet Master Unit. Preset in consecutive words the data to be transferred, as shown below. Word Bits 15 to 8 S 7 to 0 Command code (Set Explicit Message FINS command 2801.) ...

  • マニュアル

    ... message. (↑) CMND (490) S D C 5  S: First Word Address of Command Storage Area S Bit No. 15 to 8 7 to 0 Command code (Set the FINS Explicit Message command (2802).) S+1 Node address of the Slave/Master to which the Explicit Message is sent: 0 to 3F hex (0 to 63) S+2 Explicit Message service codes Write: 10, Read: 0E S+3 Class ID code (Set the CompoNet Class code of the target function.)*1 S+4 Instance ID code (Set the CompoNet Instance ID code of the target function.) S+5 Attribute ...

  • マニュアル

    ...S Sign bit (0 = positive, 1 = negative) Exponent Binary exponent, biased by -1023 Fraction Binary fraction with an implied 1 to the left of the binary point The value of a floating point number is shown below for 0 < exponent < 2047. -1 ...

  • マニュアル

    ...int i = (int)"1.23" float float f1 = (float)"1.23" float f2 = (float)"A1" d = 1000 flag = true ( non 0 equals true) s = "1000" b=1 i=1 d = 1.23 flag = true ( non 0 equals true) s = "1.23" b=1 i=1 f = 1.23 flag = true ...

  • マニュアル

    ...byte b = (byte)1.23 int i = (int)1.23 b=1 i=1 double double d = (double)1.23 d = 1.23 bool bool flag = (bool)1.23 flag = true string string s = (string)1.23 s = "1.23" byte byte b = (byte)1.23 b=1 int int i = (int)1.23 i=1 float float f = (float)1.23 f = 1.23 Expression Editor and Listen Node Software Version: 1.84 20 bool bool bool flag = (bool)1.23 flag = true string string s = (string)1.23 ...

  • マニュアル

    ...Communications cycle 2. Safety function 3. Data backup of absolute (ABS) encoder 4. Resolutions of absolute (ABS) and increment (INC) encoders G5 series 1S series ● Cycle in DC mode: ● Cycle in DC mode: 250 µs, 500 µ...

  • マニュアル

    ...Default Parameter Default SS2 to G5 settings No. Parameter name setting No. Parameter name setting [hex] [dec] [dec] [dec] Set the proportional gain of position control. 48.0/32. Pn10 Position Loop Gain 40 ...

  • マニュアル

    ...100 800 200 300 400 1000 500 600 1200 700 800 1000 Stopping Distance Zone Pair Transition 900 (1180 mm/s, 950 mm) (1200 mm/s, 973 mm) 2.5 (1140 mm/s, 1.474 s) (1070 mm/s, 1.410 s) (980 mm/s, 1.330 s) (880 mm/...

  • マニュアル

    ...s?0.h 1 -9999 to 99999 99999 Comparative set value 0L s?0.l 1 -9999 to 99999 1 -9999 Comparative set value 0LL s?0.ll 19999 to 99999 1 -9999 Comparative set value 1HH s?1.hh 19999 to 99999 99999 Comparative set value 1H ...

  • マニュアル

    ..., on off --- --- off, on off off --- --- Power supply memory Comparative set value display s?.dsp Display refresh period d.ref Display color selection color Display adjustment Setting range off, 0.5 s, 1...

  • マニュアル

    ...0002 Character Monitor/Setting range sv.dsp H’00000000: OFF(0), H’00000001: ON(1) Character Default setting Decimal point Unit off, on off --- --- d.ref H’00000000: OFF(0), H’00000001: 0.5 s(1), H’00000002: 1 s(2), H’00000003: 2 s(3), H’00000004: 4 s(4) off, 0 . 5, 1, 2, 4 off --- s Display color selection color H’00000000: Green (red)(0), H’00000001: green(1), H’00000002: red (green)(2), H’00000003: red(3) grn-r, grn, red-g, red grn-r --- --- 0003 Display value selection disp H’00000000: PV(0), H’00000001: ...

  • マニュアル

    ...value Parameter List Level Parameter name Characters Characters Initial value Decimal point Unit Comparative set value display s?.dsp OFF, ON off, on OFF Display refresh period d.ref OFF, 0.5 s, 1 s, 2 s, 4 s off, 0. 5, 1, 2, 4 OFF --- s Green (red), green, red (green), red grn-r, grn, red-g, red Green (red) --- --- Display color selection color Display adjustment Setting range --- Set value --- Display value selection disp PV, max, min p?, max, min PV --- --- Automatic display return ret 0 to 99 0 to 99 10 --- s Position meter type pos-t OFF, ...

  • マニュアル

    ... Set Point ......................... 5-23, 6-10, A-13 Temperature Stabilization Range ......... 5-23, 6-10, A-13 Use Running Time .................................. 5-29, 6-6, A-14 Voltage Input Range ............................. 5-26, 6-10, A-14 setting values ..................................................................5-4 Shift Key (...

  • マニュアル

    ...This does not include the measuring error margin of the special CT. Value when ambient temperature of 23°C, rated input, and rated frequency. 10% or more of the rated input current For the voltage between R and T phases, the accuracy is ±1.0% of F....