.... . . . . . . . . . . . . . . . Connection to Temperature Controller other than E5CN and E5GN . . . . . . . . . . . . . . . . . 5-2-1 Two-point Shift (Connection to E5AK, E5CK, or E5CK) . . . . . . . . . . . . . . . . . . 5-2-2 One-point Shift (Connection to Temperature Controller with Input Shift Function) . . . . . . . . . . . Section Connection to E5CN or E5GN 5-1 5-1 Connection to E5CN or E5GN 5-1-1 Input Shift The input shift type is displayed according to the input type of Sensor selected. • Two-point shift compensation is used for the Non-contact Temperature Sensor only. • The input temperature range is shifted by the temperature input shift value. For example, a display value ...