全 24 件が検索されました。(1 - 20件を表示)
- カタログ
... 2 50.0 SP 0 Dead Band chys Manual Reset Value Hysteresis (Heating) soak Hysteresis (Cooling) 0 wt-b Soak Time 0 mv-s SP 5 mv-e 0 sprt M sp-7 sprl SP 7 MV Upper Limit 0 M ol-l 0.0 M Work Bit 5 ON Delay MV Lower Limit M Heater Current 1 Value Monitor M r-s al3l M Leakage Current 1 Monitor al-4 Leakage Current 2 Monitor al4h Program Start al4l 0 0 o Work Bit 7 ON Delay c-o 0.0 M Alarm Value 1 v-m 0.0...
- カタログ
...助リレー1 0 OFFディレー w4of 0 M a-m 上限値1 al1l 警報 現在値/目標値(2) 0 w1of 0 0.0 M sp-7 ストップ時操作量 M 0 sp-6 mv-s 0.0 M sp-5 M w1on 内部補助リレー1 0 M sp-4 ローカット点 内部補助リレー6 0 ONディレー 1 M 0.0 0 M 目標値...
- カタログ
... 4 0 Disturbance 233 Integral Time d-i M M Disturbance 40 Derivative Time SP 5 d-d SP 6 c-db 0 M M 0 0.0 M M sp-7 SP 7 of-r 0 50.0 M M ins Process Value Input 0.0 Shift inrt hys Process Value Slope 1.000 Coefficient chys M M Input Digital Filter M w-ht off M w-il 1.4 M w-dl 0.6 M M M M PID Update (Adaptive Control) mv-s 0.0 Work Bit 2 0 OFF Delay M w3on Work Bit 3...
- カタログ
...M a-m 操作量変化率 上限値1 M 0 内部補助リレー4 0 ONディレー 233 0 M w4on M M sp-7 外乱用比例帯 8.0 0 sp-6 目標値応答用微分時間 M M sp-5 sp-d M M sp-4 目標値応答用 233 積分時間 sp-i 40 0 sp-3 sp-p 目標値応答用比例帯 8.0 M M...
- マニュアル
...chys *6 28 29 30 31 (−) EV1 EV2 32 33 34 35 36 *6 1.0 sp-6 SP 6 0 soak *6 SP 1 1 sp-7 SP 7 0 wt-b *6 off *6 SP 2 *6 ins 0.0 Process Value Input Shift mv-s *6 inrt 1.000 rss 0.0 rsrt 1.000 p 8.0 i 233 d 40 c-p 8.0 c-i 233 c-d 40 c-db SP 3 *6 0.0 mv-e Process Value *6 Slope Coefficient 50.0 Hysteresis (Cooling) Soak Time Wait Band MV at Stop...
- マニュアル
...o r-s run时 run 当控制停止=stop时当控制启动= ∗6 al-1 ∗6 al1h 0 报警值1 ∗4 ∗6 0 hb2 0.0 ∗6 sp-7 0 ∗6 ins 0.0 ∗6 inrt 1.000 0.0 报警值4 ∗4 加热器电流2值监控 (单位:A)∗7 ∗6 rss 0.0 加热器断线检测2 (单位:A)∗7 ∗6 漏电流1值监控 (单位:A)∗7 ∗6 rsrt 1.000 50.0...
- マニュアル
...sp-1 d SP 1 40 0 sp-2 c-i SP 3 233 0 sp-4 c-d SP 4 40 0 sp-5 sp-6 c-db SP 5 sp-7 Hold O and M keys down for at least 1 second 0 M oapt 0 M icpt 1 M wtpt off M pfpt off Move to Protect Level Displayed only when a password is set. Restricts moving to Protect Level. Operation / Adjustment Protect Restricts displaying and modifying menu items in Operation, Adjustment, and Manual Control Levels. Initial Setting / Communication Protect Restricts movement to the Initial Setting, Communications...
- マニュアル
...MV Monitor (Heating) sp-0 *6 HS Alarm 2 (Unit: A) *7 *6 SP 0 *6 0 sp-1 SP 1 *6 M sp-2 *6 sp-6 SP 6 0 sp-7 *6 chys 0.0 inrt 1.000 rss 0.0 SP 7 *6 soak 1 p 8.0 i 233 d 40 PV Input Shift *6 wt-b off PV input Slope Coefficient *6 mv-s 0.0 *6 M c-d 40 MV at Stop M Remote SP Input Shift *6 mv-e 0.0 MV at PV Error M Slope Coefficient *6 sprt off SP ...
- マニュアル
...检测1 hb1 (单位: A)∗5 0 al3l 0.0 加热器电流1值监控 保温时间 1 M 0.0 (单位:A)∗5 报警值3 ∗2 SP 7 M ins 通信写入 M M 漏电流1值监控 (单位:A)∗5 0 soak M off ct1 M sp-7 M 初始设定菜单可以使用户指定喜欢的工作条件(输入类型,报警类型,控制方法...
- マニュアル
...SP − 36 *6 *6 1.0 *6 *6 *6 Leakage Current 1 Value Monitor (Unit: A) *7 *6 chys *6 1.0 soak *6 RS-485 A(−) (−) 1 sp-7 SP 7 0 wt-b *6 off ins 0.0 PV Input Shift mv-s *6 0.0 inrt 1.000 mv-e PV input *6 Slope Coefficient rss 0.0 rsrt 1.000 0.0 Remote SP Input Shift sprt *6 off p sprl Remote SP input *6 Slope Coefficient same i 233 d *6 40 *6 c-p 8.0 *6 c-i 233 *6 c-d 40...
- マニュアル
...6 ∗6 ∗6 ∗6 加热器断线检测2 (单位:A)∗7 ∗6 漏电流1值监控 (单位:A)∗7 ∗6 hs2 50.0 sp-6 0 sp-7 0 ins 0.0 inrt 1.000 rss 0.0 rsrt 1.000 漏电流2值监控 p HS报警2 (单位:A)∗7 0 sp-2 ∗6 d ∗6 0 sp-3 0 ∗6 c-p 和M键至少3秒 hys ∗6 1.0 ∗6 8.0 SP 0 SP 6 ∗6 ...
- マニュアル
...运算启用(限于已经设定了模拟输入) al1l sp-4 0 sp-5 报警值下限1 ∗2 sp-6 操作时应正常使用操作菜单。 sp-7 M 按住O和M键至少3秒 ON OFF ON OFF ON OFF X X 0 X 0 X 0 ON OFF ON OFF ON OFF ON OFF ins 保护菜单 SP 2 0 SP 3 pmov 0 M M icpt 有关高级功能设定菜...
- マニュアル
...OFF OFF SP 2 OFF ON OFF SP 3 ON ON OFF SP 4 OFF OFF ON SP 5 ON OFF ON SP 6 OFF ON ON SP 7 ON ON ON Note: Any bits that are not assigned to event inputs are treated as being OFF. Using Key Operations You can select any of the set points 0 to 7 by changing the set value of the Multi-SP Uses parameter. The Multi-SP Uses parameter display conditions are as follows: • Digital Controllers without event inputs for which the Number of Multi-SP Points parameter is not set ...
- マニュアル
...0033 Alarm Value Upper Limit 4 C1 (81) 0034 Alarm Value Lower Limit 4 C1 (81) 0035 SP 4 C1 (81) 0036 SP 5 C1 (81) 0037 SP 6 C1 (81) 0038 SP 7 C1 (81) 0039 Proportional Band (Cooling) C1 (81) 003A Integral Time (Cooling) C1 (81) 3-6 003B Derivative Time (Cooling) Setting (monitor) value H'00000000 to H'000003E8 (0.0 to 100.0) Level Adjustment H'00000001 to H'00000064 (0.1 to 10.0) H'00000001 to H'000000C8 (0.1 to 20.0) H'FFFFF831 to H'0000270F (−1999 to 9999) H'00000001 to ...
- マニュアル
...OFF OFF SP 2 OFF ON OFF SP 3 ON ON OFF SP 4 OFF OFF ON SP 5 ON OFF ON SP 6 OFF ON ON SP 7 ON ON ON Note: Any bits that are not assigned to event inputs are treated as being OFF. E5@D Digital Temperature Controllers User’s Manual (H224) 5 - 33 5-8-1 Event Input Settings The following table shows the relationships between the ON/OFF status of multi-SP number switching bits 0 to 2 and the set point. Selected set point 5-8 Using Event Inputs • Events can be used ...
- マニュアル
...Enable PF Key Protect MV Change Rate Limit Extraction of Square Root Low-cut Point Alarm Value 4 Alarm Value Upper Limit 4 Alarm Value Lower Limit 4 SP 4 SP 5 SP 6 SP 7 Proportional Band (Cooling) Integral Time (Cooling) Setting (monitor) value Standard control: H'FFFFFFCE to H'0000041A (−5.0 to 105.0) Heating and cooling control: H'FFFFFBE6 to H'0000041A (−105.0 to 105.0) H'00000000 (0): OFF H'00000001 to H'0000270F (1 to 9999) Standard control: MV lower limit + 0.1 to H'0000041A (MV lower limit + 0.1 to 105....
- マニュアル
...します。 rSP2、3、6、7 ......伝送路選択ピン(ショートプラグ使用) BSD(バックSD) 対上流用 NRD (ノーマルRD) SP 6 SP 2 SP 7 SP 3 NSD(ノーマルSD) BRD (バックRD) 対下流用 2C 1 2-C間ショートで光ファイバ使用電源供給ピンの設定と合わせて行ってください。 10....
- マニュアル
...M lcr2 6-24 M M hs1 目標値 7 0 ins 6-28 M M M lcr1 6-24 M M hb2 目標値 6 0 sp-7 hys M M M ct2 6-24 M M hb1 sp-6 M SP モード lsp ct1 目標値 5 0 M off spmd sp-5 マニュアル 50.0 リセット値 M M off of-r M 0 at 参照ページ デッドバンド 0.0 M 形 E5□C デジタ...
- マニュアル
...積分時間 233 M 6-21 外乱用比例帯 8.0 M M sp-i 0 係数番号 M ins 8.0 40 微分時間 M sp-7 比例帯 8.0 比例帯 M sp-6 M 40 M sp-5 水冷用比例帯 0.6 減少閾値 233 0 sp-4 M 8.0 M sp-3 水冷用比例帯 1.4 増大閾値 40 M sp-2 M d 目標値 1 水冷出...
- マニュアル
...Setting See F Related description 3.5 Setting Patterns (page 3-14) F Related parameter All parameters in the program mode Step 0 time (Step time) Target SP 0 (Rate of rise programming) to Step 7 SP (Step time) Target ...