全 1 件が検索されました。(1 - 1件を表示)

  • マニュアル

    ...0 1 0 1 1 0 C transferred to indicate bit number 12 as the highest ON bit. Result word C For 256-bit conversion, DMPX(111) determines the position of the highest ON bit in SB to SB+15, encodes it into two-digit hexadecimal value corresponding to the bit number of the highest ON bit, then transfers the hexadecimal value to the specified 8-bit digit in R. The first digit to receive the results is specified in Di, which also specifies the number of digits to be encoded. The following is an example of a one-digit ...