全 1370 件が検索されました。(1221 - 1240件を表示)
- マニュアル
... Read/Write Head (R/W Head, Electromagnetic Coupling) V600-series Data Carrier (DC) Read/Write Head Connector Peripheral Port (See note) RS-232C Port (See note) Note These ports can be connected to a Programming Console (CQM1-PRO01-E or ...
- マニュアル
...Section 4-5 SRM1-C0@-V2 Master Control Units Item RS-232C port Specifications 1 port (SRM1-C02-V2 only) Host link, NT link, 1:1 PLC link, ASCII data transfer with XON, XOFF flow control Programming Console (CQM1-PR001-E/...
- マニュアル
... can be used on the CPU Rack or Expansion I/O Rack under the C200Hj-CPUjj-(Z)E. They cannot be used on Slave Racks. 2. Each 64 I/O Unit is treated as two Units. 3. Special I/O Units like the C200H-NC211 that are allocated the words for two Units are treated as two Units. 4. Unit number settings for Group-2 Units for the following CPU Units must be between 0 and 9: C200HE-CPU32/42-E/ZE C200HG-CPU33/43-E/ZE C200HX-CPU34/44-E/ZE 5. Group-2 High-density I/O ...
- マニュアル
...). • Starting/stopping data links (Start Bit: ON/OFF) • Programming for the message service. • Reading (monitoring) the network status. Programming Device CX-Programmer (for PLC) Programming Console External appearance Model WS02-CXPC@-EV@ CQM1-PRO01-E ...
- マニュアル
... and 32 internal outputs points are supported for each Unit, and up to 3 Units can connected. DeviceNet application allows networks to be constructed including devices from other manufacturers. Standard Peripheral Devices The CPM1A uses the same Programming Consoles and SYSMAC Support Software (SSS) as the ...
- マニュアル
... Programming Console. Refer to 5-5 Programming Console Operation Errors for details on errors that might occur during Programming Console operations. 4-1-1 Compatible Programming Consoles There are two Programming Consoles that can be used with the SRM1: the CQM1-PRO01-E and the ...
- マニュアル
... is a Programming Device for CS1-series PCs and C/CV-series PCs and is used with the CV500-MC221, CV500-MC421, C200HMC221, CS1W-MC221, and CS1W-MC421 Motion Control Units. Please read this manual carefully along with the operation manuals for the CV500-MC221, CV500-MC421, ...
- マニュアル
... can be used with the SYSMAC-NCT Support Tool. Applicable Position Control Units Corresponding PCs C200HW-NC113/213/413 C200HX/HG/HE(-Z) PCs C500-NC113/211 C-series and CV-series PCs Note The SYSMAC-NCT Support Tool cannot be used with ...
- マニュアル
...1_ocations SIOUUnits (ReadOn]y) Group2]【ノO Units(Read Only) LocaERacks SYSBUS RemoteRacks SYSBUS RemoteU㎡ts SYSBUS12 GrouplU皿its SYSBUS/2 Gmup2Units SYSBUS/2 Group3U皿its Rack Type C200H C500 58M 54M 122M CV CVM1 LK,SN,SL,BA,ET, MC,VP,SM,ME,MI, IS,DN,RM# ."譲纏㌶ 難 ㌶灘熱灘 ㌶"・."、÷◇w 鱗 、. 、. ぺ. 熟 ". " シ芯糠襟鍵 〆 ・懸・懸 s.・、㌔NN.'弍⇔LR.:〉 灘 o,i,O,1,00,H, OOOO,皿OI,OOII GG N,NN,NNNN LL,GL HH INTn RMn #[SIOU] 難懸議酬 、、㌔ 黙...
- マニュアル
... outputs being turned OFF. As a countermeasure for such problems, external safety measures must be provided to ensure safety in the system. ! Caution xiv Tighten the screws on the terminal block on the AC Power Supply Unit to the torque specified in the ...
- マニュアル
...-mode command Note 1. There are two Host Link formats: the 1:N Host Link (with N 1) and the 1:1 Host Link. • The 1:1 Host Link is the earlier Host Link format supported by C-series PLCs, such as the ...
- マニュアル
...@@H, CJ1M-CPU@@, CJ1G-CPU@@ Programmable Controllers Instructions Reference Manual Describes the ladder diagram programming instructions supported by CS-series and CJ-series PCs. xi About this Manual, Continued Name Cat. No. Contents SYSMAC CS/CJ-series ...
- マニュアル
.... . . . . . . . . . . . . . . . 215 SECTION 6 Special I/O Slave Units Specifications. . . . . . . . . . . . . . . . . . 229 6-1 C200H I/O Link Units . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 230 6-2 RS-232C Units. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 260 SECTION 7 Communications Timing . . . . . . . . . . . . . . . . . . . . . . . . . . . . 299 7-1 Remote I/O Communications Characteristics . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 300 7-2 Message Communications Time . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 309 SECTION 8 Troubleshooting and Maintenance . . . . . . . . . . . . . . . . . . . . 311 8-1 Indicators and Error Processing. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 312 8-2 Troubleshooting . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 313 8-3 Maintenance. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 318 Appendices A Node Address Settings Table. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 321 B Using Another Company’s Master Unit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 323 C Connectable Devices and Device Current Consumptions . . . . . . . . . . . . . . . . . . . . . . . . . . 343 D Precautions when Connecting Two-wire DC Sensors . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 353 Glossary . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 355 Index. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ....
- マニュアル
...CVM1-PRS21-V1E Programming Console Operation Manual W222 CompoBus/D Master Unit CVM1-DRM21-V1 CompoBus/D Master Unit Operation Manual W267 Controller Link Unit CVM1-CLK21 Controller Link Unit Operation Manual W309 Controller Link Support Software ...
- マニュアル
...Programming Console Operation Manual CompoBus/D Master Unit CVM1-DRM21-V1 CompoBus/D Master Unit Operation Manual W267 Controller Link Unit CVM1-CLK21 Controller Link Unit Operation Manual W309 Controller Link Support Software SYSMAC NET Link Unit ...
- マニュアル
... connected. DeviceNet application allows networks to be constructed including devices from other manufacturers. 3 Section CPM2A Features and Functions Share Programming Devices 1-1 The same Programming Devices, such as Programming Consoles and Support Software, can be used for the ...
- マニュアル
... external device. The one connector support two different ports: Peripheral and RS-232C. CPM2C CPU Unit Peripheral port (CMOS level) RS-232C port (RS-232C) Use the correct Connecting Cable (CPM2C-CN111, CS1W-CN114, or CS1W-CN118). Note a) A ...
- マニュアル
...IBM PC/AT or compatible Ladder Support Software, SYSMAC Support Software CPU Unit XW2Z-@@@S(-V) RS-232C port Note You can also connect to the RS-232C port on a Serial Communications Board. Programming Console CQM1-PRO01-E ...
- マニュアル
... from an existing Host Link System to one using an RS-232C port on a CQM1H-series CPU Unit or Serial Communications Boards. Previous products C-series Host Link Units Model number 3G2A5-LK201-E C500-LK203 3G2A6-LK201-E ...
- マニュアル
.... . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 147 9-3 Using the C200H-SLK21 or C1000H-SLK21. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 148 SECTION 10 Inspection and Maintenance . . . . . . . . . . . . . . . . . . . . . . . . . 149 10-1 Periodic Inspections. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . viii 150 10-2 Handling Precautions. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 150 10-3 Tools and Equipment Needed for Inspection. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 150 TABLE OF CONTENTS Appendices A Standard Models . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 151 B Dimensions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 153 C Related Auxiliary Area Information . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 155 D CPU Bus Unit Area Allocations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 157 E DM Area Allocations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 161 Glossary . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 163 Index . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 179 Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 181 ix About this Manual: This manual describes the installation and operation of CS-series SYSMAC LINK Units and includes the sections described below. Please read this ...