全 90 件が検索されました。(81 - 90件を表示)
- マニュアル
... combined with the memory area codes to specify memory locations. The No. of bytes column specifies the number of bytes of data to read or write for that area. Area CIO area Expansion CIO area LR area Data type ...
- マニュアル
... B7A Interface Unit. 16-point B7A Link Terminals, 32-point B7A Link Terminals with a two-circuit configuration, and Mixed I/O B7A Link Terminals with a 16-point input/output configuration can be connected. Comparison between Standard and Group-2 B7A Interface Units Type ...
- マニュアル
... Link Terminals. The 16-point B7A Link Terminals include 16-point (non-mixed) Terminals, 32-point Terminals configured with two 16-point circuits, and mixed-I/O Terminals with 16 inputs and 16 outputs. Comparison between Standard and Group-2 B7A Interface Units Type ...
- マニュアル
... 16-point B7A Link Terminals. 16-point B7A Link Terminals include 16-point (input or output) models, models with 2 circuits configured with 16 points, and models with 16 points of mixed I/O. Comparison between Standard and Group-2 B7A Interface Units Type ...
- マニュアル
... 1-1 Functions 1-1-3 Communications Board Models The following Communications Boards are available. The features that are to be used from among those listed below as “YES” for any particular Communications Board is specified in the PC Setup at startup. Type ...
- マニュアル
...y Start Bit 03 04 Single Block Forced Block End 05 Pause 06 M Code Reset Bit 07 Program Number Read Bit Teaching Address Set Bit Teaching Bit Teaching g Type yp Bit 08 09 10 All tasks common 1 n+2 00 to 15 11 12 13 14 15 0 ↑ 1 0 1 ↑ 1 ↑ 1 ↑ 1 Any axes operating in manual mode will decelerate to a stop. Automatic mode When the MC program is being executed, it will be stopped and any operating axes will decelerate to a stop. ↓ 1 Manual mode Starts MC program execution. Continues MC program ...
- マニュアル
...・∵ 一・A…三 、 ニ】▲■ キ4.,工 ード, r'r 1'Z' ' ' ぷ福1蹴麓恨R笥輿口書 フー ジ コ ピ ニノノコノ コノ㎞ぱd㎏r下yp伊 None こ,!/∵一、 ▲ ' ●o Rene ::、ン■ン∴、1∴ ご寺 ⑳ ▼ ▼ ▲ ,▲None.罰 、 一 = ■i 一 一む ▲一 , 一 , 、wnLWLS"va"Ws∨V"■S-.LVL9 ' ㌦十…∴…元i/ll!li考証▲㍉「.「"i}・〃 悟㍉「1〔llii三ワ ノ ゴぐ ビ グ へ ヘピ ヘシ ぐミきザ三:▼一.已1璽・...
- マニュアル
... in the CX-Process Tool as shown below. • Example: CX-Programmer Symbol Table 145 User Link Tables Section 3-5 • Imported User Link Table Data Imported from CX-Programmer Symbol Table CX-Programmer local symbol table Symbol name Type ...
- マニュアル
...A double precision variable that indicates the Y coordinate of the center of gravity of the standard object registered in the specified scene. Use the STDSET or SSTDSET statement to register the Y coordinate of the center of gravity of a certain object to this variable. ...
- マニュアル
... setting) YM Trigger + 450 ms (minor setting) YJ Trigger + 650 ms (minor setting) YN Trigger + 500 ms (minor setting) YK Trigger + 700 ms (minor setting) YO Trigger + 550 ms (minor setting) YL Trigger + 750 ms (minor setting) ...