全 622 件が検索されました。(61 - 80件を表示)

  • カタログ

    ... DC24V 61F-LS-CP11-BTC 61F-GP-N8 AC@@V 61F-LS-CP08-NRA 61F-GP-N AC@@V 61F-LS-CP11-NRA Long-distance wiring 2 km 61F-GP-N8L 2KM AC@@V 61F-LS-CP08-NRA 61F-GP-NL 2KM AC@@V 61F-LS-CP11-NRA Long-distance wiring 4 km 61F-GP-N8L 4KM AC@@V 61F-LS-CP08-NRA 61F-GP-...

  • カタログ

    ...promoted as a standard by the Special Committee for Network. Promotion organized by JEMA (The Japan Electrical Manufacturers' Association). FL-net enables multivendor, multi-model connections at the controller/machine level. FL-net provides the following features. z Ethernet-based FA Network • ...

  • カタログ

    ...promoted as a standard by the Special Committee for Network. Promotion organized by JEMA (The Japan Electrical Manufacturers' Association). FL-net enables multivendor, multi-model connections at the controller/machine level. FL-net provides the following features. z Ethernet-based FA Network • ...

  • カタログ

    ... 20 mA ±5 V ±10 V Setting range Values from −19999 to 99999 can be displayed with scaling. The position of the decimal point can be set as desired. Note: The default value is 4-20: 4 to 20 mA input range. K3GN-...

  • 技術解説/使用上の注意事項

    ... 他 M 共通事項 お問い合わせ 0120-919-066 最新情報は www.fa.omron.co.jp 37 電力・機器用保護機器 技術解説 N NL 例 符号 変圧器 26T 変圧器温度継電器 窒素 63N 窒素圧力継電器 放水路 33T 放水路用液面検出器 中性 64N 中性点地絡過電圧継電器 温度 43T 温度(自...

  • 技術解説/使用上の注意事項

    ...回路 E5、E6回路 セ ーフティ ⑥絶縁不良があればその配線を取り替える。 ⑦長い配線が必要な場合は遠距離用(形61F-□NL(-□L) の2kmまたは4km)と交換する。 誘導による誤動作であればシールド線を使用するか別配線にする。 ⑥次の電極回路の配線に絶縁...

  • マニュアル

    ...要となります。 ■製造者およびEU代理人製造者 : OMRON Corporation 京都市下京区塩小路堀川東入 EU代理人 : Omron Europe B.V. Wegalaan 67-69, NL-2132 JD Hoofddorp, The Netherlands はじめに 取付手順 配線方法 EtherCAT通信ユニット形 3G3AX-RX2-ECTは、オムロン製インバータ (RX2シリーズ)に内蔵することにより、...

  • マニュアル

    ... the ferrite core to each EtherCAT communications cable. • This is a Class A product. In residential areas it may cause radio interference, in which case the user may be required to take adequate measures to reduce interference. Omron Europe B.V. Wegalaan 67-69, ...

  • マニュアル

    ... THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(S) IS PROPERLY RATED AND INSTALLED FOR THE INTENDED USE WITHIN THE OVERALL EQUIPMENT OR SYSTEM. OMRON EUROPE B.V. (Importer in EU) Wegalaan 67-69, ...

  • マニュアル

    ... THAT THE SYSTEM AS A WHOLE HAS BEEN DESIGNED TO ADDRESS THE RISKS, AND THAT THE OMRON PRODUCT(S) IS PROPERLY RATED AND INSTALLED FOR THE INTENDED USE WITHIN THE OVERALL EQUIPMENT OR SYSTEM. OMRON EUROPE B.V. (Importer in EU) Wegalaan 67-69, ...

  • マニュアル

    ... AND INSTALLED FOR THE INTENDED USE WITHIN THE OVERALL EQUIPMENT OR SYSTEM. OMRON EUROPE B.V. (Importer in EU) 3 4 5 6 (TOP VIEW) • Mounting hole machining dimensions 2-M4 or φ 4.5 hole Wegalaan 67-69, ...

  • マニュアル

    .... Ethernet Unit (100Base-TX Type) CJ1W-ETN21 Operation Manual Construction of Networks W420 OMRON Corporation (Manufacturer) Shiokoji Horikawa, Shimogyo-ku, Kyoto, 600-8530 Japan Contact: www.ia.omron.com Regional Headquarters OMRON EUROPE B.V. (Importer in EU) Wegalaan 67–69, ...

  • マニュアル

    ...W472 Hardware User’ s Manual Cat. No. Ethernet Unit (100Base-TX Type) CJ1W-ETN21 Operation Manual Construction of Networks W420 OMRON Corporation Industrial AutomationCompany Tokyo, JAPAN Contact: www.ia.omron.com Regional Headquarters OMRON EUROPE B.V.Wegalaan 67–69, ...

  • マニュアル

    ...우려가 있습니다. OMRON Corporation (Manufacturer) Shiokoji Horikawa, Shimogyo-ku, Kyoto, 600-8530 Japan Tel: (81)75-344-7109 Fax: (81)75-344-7149 Regional Headquarters OMRON EUROPE B.V. (Importer in EU) Wegalaan 67-69, ...

  • マニュアル

    ... in the relevant manual. Improper installation of the Unit may result in malfunction. OMRON Corporation (Manufacturer) Shiokoji Horikawa, Shimogyo-ku, Kyoto, 600-8530 Japan Contact: www.ia.omron.com Regional Headquarters OMRON EUROPE B.V. (Importer in EU) Wegalaan 67–69, ...

  • マニュアル

    .... Japan Tel: (1)847-843-7900 Tel: (81)55-977-9181 Fax: (1)847-843-8568 Fax: (81)55-977-9045 "#'&$ )-*, *+ 83 Clemenceau Avenue, #11-01, UE Square, Singapore 239920 Wegalaan 67-69, Tel: (65)6835-3011 ...

  • マニュアル

    ... Locations subject to exposure to water, oil, or chemicals • Locations subject to shock or vibration z Connect the adapter to the compatible models. Risk of damage if a noncompatible model is connected. Contact: www.ia.omron.com OMRON EUROPE B.V.Wegalaan 67-69, ...

  • マニュアル

    ... Commands Reference Manual W342 OMRON Corporation Control Devices Division H.Q. Shiokoji Horikawa, Shimogyo-ku, Kyoto, 600-8530 Japan Tel: (81)75-344-7109 Fax: (81)75-344-7149 Regional Headquarters OMRON EUROPE B.V. Wegalaan 67-69, ...

  • マニュアル

    ... Series Communications Commands Reference Manual OMRON Corporation Control Devices Division H.Q. Shiokoji Horikawa, Shimogyo-ku, Kyoto, 600-8530 Japan Tel: (81)75-344-7109 Fax: (81)75-344-7149 Regional Headquarters OMRON EUROPE B.V. Wegalaan 67-69, ...

  • マニュアル

    ...U.S.A. Tel: (1)847-843-7900 Fax: (1)847-843-8568 Regional Headquarters OMRON ASIA PACIFIC PTE. LTD. OMRON EUROPE B.V.(Importer in EU) 83 Clemenceau Avenue, Wegalaan 67-69, #11-01, UE Square, Singapore 239920 ...