全 863 件が検索されました。(541 - 560件を表示)

  • マニュアル

    ...C200HX-CPU34/44/54/64/65/85ZE --C200HW-COM02/04/ 05/06-EV1 C200HS C200HE C200HE-Z C200HG C200HG-Z --- C1000H-CPU01-EV1 C2000H-CPU01-EV1 C1000H-CPU01-EV1 C1000HF-CPU01-EV1 C2000H-CPU01-EV1 --- C500-LK201-EV1 --- --- --- --- CPM2A --- --- CPM2C --- --- CQM1 CQM1H-CPU51/61 CQM1H-SCB41 CQM1H C Series ----- --- CPM1-10/20/30CDR-@ +CPM1-CIF01 CPM1A-10/20/30/40CD@-@ +CPM1-CIF01 CPM2A-30/40/60CD@@-@ +CPM1-CIF01 (Peripheral port connection) CPM2C-10/20@@@@@@-@ (*2) CQM1-CPU21-E CQM1-CPU41/42/43/44-EV1 CQM1H-CPU11/21/51/61 (*3) Host Link Unit or Communications Board/Unit Connectable to C200HX...

  • マニュアル

    .../64/ 65/85-ZE C1000H-CPU01-EV1 C2000H-CPU01-EV1 C1000H-CPU01-EV1 C1000HF-CPU01-EV1 C2000H-CPU01-EV1 C200HW-COM02/04/ C200HS 05/06-EV1 C200HE C200HE-Z C200HG C200HG-Z C200HX C200HX-Z C500-LK201-EV1 C1000H C2000H ...

  • マニュアル

    ... supplied as a standard accessory with the NT Support Tool (NT-ZJCAT1-EV4). 22 Section System Configuration 1-3 Reference: The following optional devices are available. Reflection-suppressing Protective Sheets (5) Chemical-resistant cover Battery NT20S-KBA04 NT20S-KBA01 ...

  • マニュアル

    ...FORCED SET/RESET CANCEL Applicable PLCs The following PLCs support the SYSWAY protocol. (Not all of the above FINS commands are supported by each of the PLCs.) C20, C50, C120, C120F, C20H/C28H/C40H/C60H, C20P/C28P/C40P/C60P, C20PF/C28PF/C40PF/C60PF, ...

  • マニュアル

    ...線式センサなど) TRG1 2.2kΩ TRG2 2.2kΩ 0V(COM) +V ●NPNトランジスタ出力 RST 2.2kΩ 内部回路 ) 内部回路 ( C200H-OD21, C500-OD412など 内部回路 +V ●PLC出力ユニット 内部回路 COM_I 出力 0V DC 24V + 電源 ●有接点タイプ ・出力部 ( C200H-ID212, ...

  • マニュアル

    ...Shielded twisted pair cable Input A + A+ – A– + B+ – B– + C+ – C– Input B Input Z E The following wiring example shows connections between an open-collector encoder and an Encoder Adapter (C500-AE001), and between the Encoder Adapter and inputs A, B, and Z. Connections should be wired so that Counter Unit inputs go ON when encoder outputs go ON. Because the ...

  • マニュアル

    ... product, or product failure. Please read each section in its entirety and be sure you understand the information provided in the section and related sections before attempting any of the procedures or operations given. ix PRECAUTIONS This section provides general precautions for using the ...

  • マニュアル

    ...14 21 22 The following table lists the applications and applicable models for each of the OMRON crimp connectors shown above. Model Number Application Applicable Models Connection S3200-COCH62M SYSMAC NET Link nodes S3200-LSU03-01E Line Server, ...

  • マニュアル

    ... SYSMAC LINK Unit and one Rack-mounting Host Link Unit In addition to the Units in the above combinations you may also mount one CPU Unit-mounting Host Unit or up to two PC Link Units. Only one PC Link Unit can be mounted on the ...

  • マニュアル

    ... next to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the C120, ...

  • マニュアル

    ... slots next to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the ...

  • マニュアル

    ...fromeachgroupmustsatisfyboththefollowingequations: 3A+B+2C+6D≦12 A+B+C+D≦8 2.OtherUnitscanbeaddeduntilthetotainumberofUnitsreachesten.lfPC LinkUnitsareused,thenumberefUnitsincludingthePCLinkUnitsmust notexceedten. P『ecaUttons TheIRareaoftheC200HSpeciall!OUnitisallocatedaccordingtethesettingof theunitnumberswitchonthefrontpanel,nottheaddressoftheslotwherethe unitismounted.Referto4・1MθmoryAlloCatiOnfortheallocationofthememOry area. LeavethetwoslotsnexttotheCPUfree.ltisnotpossibletotLsedev▲cesconnectedtotheCPU(suchastheProgrammingConsole)iftheseslotsareOccupied. lftheC200HSIaveRackisconnectedtoanotherSYSMACmodelRemotel/O MasterUnit,suchastheCl20,...

  • マニュアル

    ... to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the C120, ...

  • マニュアル

    ... each slot. There are 3, 5, 8, or 10 slots available on the Backplane depending on the model of Backplane used. 5. Unit Connectors Connect I/O Units, Special I/O Units, Interrupt Input Units, and/or Analog Timer Units. Note Attach a ...

  • マニュアル

    ...C200H-CN222/422 (2 m/4 m) XW2Z-200S/500S (See note) Programming Console Connecting Cable Connecting Cable Peripheral Device Support Software IBM PC/AT or Compatible Peripheral port CQM1-CIF02 Connecting Cable ...

  • マニュアル

    ... the encoder to the High-speed Counter Unit through a long cable or to wire the cable in places where noise may be generated. An open collector output from an encoder can be connected as a line driver input to the High-speed Counter Unit through the ...

  • マニュアル

    ...4-2 CPU Backplane C200HW-BC031/BC051/BC081/BC101 Teaching Box CVM1-PRS71 Personal computer for SYSMAC Support Software IBM PC/AT or compatible SYSMAC Support Software Personal computer for MC Support Software MC Support Software ...

  • マニュアル

    ...C200H-CN422 C200H-ATT01 WS02-CXPC1-E C200H-PRO27-E Connecting g C bl Cable Cable length: 2 m Cable length: 4 m For panel mounting. MS-Windows 95/98 (CD-ROM) for Ver. 2.0 or higher C500-ZL3AT1-E SYSMAC Support Software 3.5”, 2HD for IBM PC/AT compatible WS01-CPTB1-E SYSMAC-CPT For IBM PC/AT or compatible computers (3.5” disks (2HD) and CDROM) CPM1-EMU01-V1 Expansion Memory Unit Uploads the ladder program and DM 6144 to DM 6655 from the PC to the EEPROM and downloads the ladder program and DM 6144 ...

  • マニュアル

    .... . . . . . . . . . Editing Sequence Data: C200HW-NC113/213/413 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Positioning Actions: C500-NC113/211 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Speed Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Acceleration/Deceleration Time and Pattern Data . . . . . . . . . . . . . . . . . . . . . . . . Editing Dwell Time Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Editing Zone Data: C200HW-NC113/213/413 . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 5 Transferring and Verifying Data . . . . . . . . . . . . . . . . . . . 5-1 5-2 5-3 Transferring Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Verifying Data . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Writing Data to Flash Memory/EEPROM . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . SECTION 6 Monitoring the Position Control Unit . . . . . . . . . . . . . . . 6-1 6-2 6-3 6-4 6-5 Overview . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . PCU Monitor Screen . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Multimonitor (C200HW-NC113/NC213/NC413) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Command Status (...

  • マニュアル

    ... adjacent to the CPU Unit. Doing so would prevent peripheral devices such as the Programming Console from being connected. Special I/O Units cannot be used on a C200H Remote I/O Slave Rack if the Slave Rack is connected to different PC (i.e., ...