全 9006 件が検索されました。(5401 - 5420件を表示)

  • マニュアル

    ... immediately execute a specific function in any Teaching Box mode. Section Nomenclature and Functions 1-4 Key Functions Classification Mode keys Key MON ORIG SRCH JOG MPG PROG EXEC EXT Direct co a d keys eys command Other keys OVERRIDE TEACH DEC STOP Function Monitors current position or I/O signals (MONITOR mode). Moves the selected axis to the origin (ORIGIN SEARCH mode). Jogs the selected axis (JOG mode). Designates the axis and multiplication factor when using a manual pulse generator (MPG mode). Executes programs (RUN mode). Sets the control mode for the MC Unit, force-locks/unlocks the ...

  • マニュアル

    ... Drive, Schaumburg, IL 60173 U.S.A. Tel: (1)847-843-7900/Fax: (1)847-843-8568 OMRON ASIA PACIFIC PTE. LTD. 83 Clemenceau Avenue, #11-01, UE Square, Singapore 239920 Tel: (65)6835-3011/Fax: (65)6835-2711 OMRON (CHINA) ...

  • マニュアル

    ...TopicsCreatingMnemonicPrograms 3 PressENTERoranarrowkeytovalidateyourentry. Iftheinformationisaccepted,itappearsintheblueareaincapitalletters.If not,theblueareagoesblank. ChoosingMenuCommandsYoucan丘ndmenucommandsformnemonic instuctionsintheMnemonicmenu.ThismenuisonlyavailableinMnemonic view. 盟II`任;1``臼..− Contactsθ−Coilsb− Functions..,一旦ungComment' Di廿erentiateトーImmediateUpdate Figu『e5・2MnemonicMenu 掴TochooseMnemonicinstructionsfromme皿...

  • マニュアル

    ... PlacesaNom司lyOpenCoilonarung. Table5・3LadderViewToolbarltems 61 ---------------------[End of Page 4004]--------------------- Part2ProgrammingPLCs Button Name Effect 顎1欄" NCCoil PlacesaNormallyαosedCoilonarung. .感 PlaceUne Placesalinetocompletearung. 轟 EraseLine Removesaline. ミ撫丁釦mer Placesatimerfunctiononamng. ■.彊』讃,酬 ...

  • マニュアル

    ...17.4 VDC min. OFF voltage 5.0 VDC max. ON response time 1 ms max. (0.1 ms max.: Interrupt input) OFF response time 1 ms max. Item Connection Terminal External signal iss open-collector ope co ec o signal X/Z Axis External signal is s line-driver ed e signal X/Z Axis Y/U Axis Y/U Axis Specification Response Time A15 A14 B15 B14 Conform to above input specifications spec ca o s N.O. contact: 0.1 ms 0 s max. a C contact: N.C. 1 ms max. A16 A14 B16 B14 Signal ...

  • マニュアル

    ... Drive, Schaumburg, IL 60173 U.S.A. Tel: (1)847-843-7900/Fax: (1)847-843-8568 OMRON ASIA PACIFIC PTE. LTD. 83 Clemenceau Avenue, #11-01, UE Square, Singapore 239920 Tel: (65)6835-3011/Fax: (65)6835-2711 OMRON (CHINA) ...

  • マニュアル

    ... terminals must be used for the power supply cable. The applicable M3 crimp terminals and recommended products are shown below. 6.2 mm max. 42 6.2 mm max. Section 3-6 Connecting to the Network Maker J.S.T.MFG....

  • マニュアル

    ...information. Note Indicates information of particular interest for efficient and convenient operation of the product. 1,2,3... 1. Indicates lists of one sort or another, such as procedures, checklists, etc. Trademarks and Copyrights COMBICON is a registered trademark of Phoenix Contact GmbH & ...

  • マニュアル

    ... show means of reducing noise. 1,2,3... 1. Noise from the communications cable can be reduced by installing a ferrite core on the communications cable within 10 cm of the DeviceNet Master Unit. Ferrite Core (Data Line Filter): LF130B (Manufactured by Easy Magnet ...

  • マニュアル

    ... USE”) occurs in the active CPU Unit during duplex initialization. The following table shows the execution timing and processing that occur during duplex initialization. (UM is the Program Area and IOM is I/O memory.) Execution Timing g FINS comman FI ...

  • マニュアル

    ... AR 1108 (comparison in progress), check AR 1109 (high-speed counter PV overflow/underflow), or execute PRV(62). Check AR 1100 to AR 1107. Supported. Not supported. --- Section Comparison with the CPM1A Item Pulse output control ...

  • マニュアル

    ...-5302 U.S.A. Tel: (1) 847-843-7900/Fax: (1) 847-843-7787 OMRON ASIA PACIFIC PTE. LTD. No. 438A Alexandra Road # 05-05/08 (Lobby 2), Alexandra Technopark, Singapore 119967 Tel: (65) 6835-3011/Fax: (65) 6835-2711 OMRON (CHINA) ...

  • マニュアル

    ...8 – SG 9 9 SG Recommended Cables UL2464 AWG28x5P IFS-RVV-SB (UL-approved, Fujikura Ltd.) AWG28x5P IFVV-SB (not UL standard) (not UL-approved, Fujikura Ltd.) UL2464-SB (MA) 5Px28AWG (7/0.127) (UL-approved, Hitachi Cable, Ltd.) ...

  • マニュアル

    ... ESD) or equivalent One Socket and one Hood are provided for each port. Recommended Cables UL2464 AWG28×5P IFS-RVV-SB (UL-approved, Fujikura Ltd.) AWG28×5P IFVV-SB (not UL-approved, Fujikura Ltd.) UL2464-SB (MA) 5P×28AWG (7/0.127) (UL-approved, Hitachi Cable, Ltd.) ...

  • マニュアル

    ...6.2 mm max. 30 6.2 mm max. Backup power supply Section 2-4 Cable Connections Recommended Crimp Terminals Manufacturer Model Japan Crimp Termi- V1.25-N3A nals KK V1.25-MS3 MOLEX JAPAN CO., LTD. VSY1.25-3.5L RAV1.25-M3 Note Remarks Suitable wiring range Vinyl insulated forked terminal Vinyl insulated round terminal Vinyl insulated forked terminal 0.25 to 1.65 mm2 (AWG #22 to #16) 0.3 to 1.65 mm2 (AWG #22 to #15) Vinyl insulated round terminal (1) Always turn OFF the power to the PLC and the backup power supply before ...

  • マニュアル

    ....A. Tel: (1) 847-843-7900/Fax: (1) 847-843-7787 Authorized Distributor: OMRON ASIA PACIFIC PTE. LTD. No. 438A Alexandra Road # 05-05/08 (Lobby 2), Alexandra Technopark, Singapore 119967 Tel: (65) 6835-3011/Fax: (65) 6835-2711 OMRON (CHINA) ...

  • マニュアル

    ....A. Tel: (1) 847-843-7900/Fax: (1) 847-843-7787 Authorized Distributor: OMRON ASIA PACIFIC PTE. LTD. No. 438A Alexandra Road # 05-05/08 (Lobby 2), Alexandra Technopark, Singapore 119967 Tel: (65) 6835-3011/Fax: (65) 6835-2711 OMRON (CHINA) ...

  • マニュアル

    ... select FinsGateway at startup. Using FinsGateway Select FinsGateway as the communications driver. Using CX-Server Select CX-Server as the communications driver. 1-6-3 Using FinsGateway Regardless of the connection method, use FinsGateway as the communications driver. Communications network Serial ...

  • マニュアル

    ...parameters) or analog signal (including parameters) DO Terminal Settings from Computer (block 401)/AO Terminal Settings from Computer (block 402), or DO Terminal to all nodes (block 407)/AO Terminal to all nodes (block 408) DO Terminal Settings from Resend signal ...

  • マニュアル

    ...A14 Signal Input common PK564AW stepping motor – CW CCW output (with 1.6-k A8 resistance) 24-V power supply for output A1 Origin Input signal Example: DFU1514W stepping motor driver, made by Oriental Motor ...