全 2436 件が検索されました。(501 - 520件を表示)

  • マニュアル

    ....RcvDat 16#0000 SktTCPRcv _instance.Done SktTCPRcv _instance.Error SktTCPRcv _instance.ErrorID 16#0000 16#**** Local_ErrCode.b[9] Timeout Output_sktCmds ErrorID 16#0000 16#**** SktClose _instance.Busy (Error end) ...

  • マニュアル

    ...an error. 4.2. Response code Sets the response code corresponding to the error in the setting response code storage area when an error occurs. Additional Information Refer to 9.8 Error Process in this document for details on the response codes. ...

  • マニュアル

    ..._EV10 0.NVF - I/O Cable FQ-WD[][] DC24V Power Supply Version Ver.1.03 Ver.1.0 Ver.1.04 Ver.3.53 Ver.1.00 Ver.1.00 - FQ2-S30-13M Ver.1.61 Ver.1.60 FQ-AC1 Precautions for Correct Use To use the configuration files, obtain the latest "Sysmac Studio project file" and "Network Configurator version 3 network configuration file" from OMRON beforehand. (To obtain the files, contact your OMRON representative.) 6 5. Applicable Devices and Support Software Precautions for Correct Use Update the Sysmac Studio to the version specified in this section or ...

  • マニュアル

    ....................................................................................................... 46 9.1. Overview .......................................................................................... 46 9.2. Communications sequence.............................................................. 50 9.3. Error Detection Processing .............................................................. 51 9.4. Memory Maps .................................................................................. 52 9.5. Ladder program ............................................................................... 55 9.6. Protocol macro data ......................................................................... ...

  • マニュアル

    ...Process. Description End Ends the communications sequence Next Moves to the next step No Abort Interrupts the step and ends the communications sequence Goto Moves to the specified step number Matrix Uses the settings of the matrix ...

  • マニュアル

    ... the last data. This timer is set to 3 seconds in this protocol macro data. Additional Information Refer to Section 4-5 Calculation Method of Monitoring Time of the CX-Protocol Operation Manual (Cat. No. W344) for the calculation method of monitoring time. ...

  • マニュアル

    ..._RDCODE. Command "Z" Number Remarks of bytes Header 1 Fixed: (16#1B) "Z" 1 Fixed: "Z" (16#5A) (Reading Trigger (destination device command)) Terminator * 1 Fixed: (16#0D) 61 9. Program 9.6.6. Receive Message Settings This section describes the settings of the receive message. Additional Information Refer to 3-4 Communication Message Attributes of the CX-Protocol Operation Manual (Cat. No. W344) for details on receive message settings. [Receive message setting screen] ●Setting of receive message RV_RDCODE (W(1),*)+ (1) (2) No. (1) Code (W(1),*) Description Message data: Variable...

  • マニュアル

    ..., and click the OK Button. *If 192.168.250.1 or 192.168.250.2 is not displayed on the dialog box, click the Add Button to add the address. *The displayed addresses depend on the status of the Network Configurator. ...

  • マニュアル

    .... Response code clear Clears the error code storage area to 0. 1.2. Operand setting for Sets execution parameters (operands) of the PMCR PMCR instruction instruction. Send/receive symbol Initializes the receive data storage area. 1.3. setting ...

  • マニュアル

    ...OMRON Sensor Head ZW-S7030 OMRON OMRON Calibration ROM (Supplied with Sensor Head) S8VS-06024 - 24 VDC power supply (for Sensor Version Ver.2.0 (Ver.2.12) Ver.1.00 Ver.4.[][] Ver.9.61 Ver.3.59c Ver.2.020 Controller) (24 VDC, 2.5A, 60W) Precautions for Correct Use Update CX-Programmer and Network Configurator to the version specified in this Clause 5.2. or to a higher version. If you use a version higher than the one specified, the procedures and related screenshots described in Section 7. and subsequent sections may not be applicable. In that ...

  • マニュアル

    .... PLC Setup ........................................................................................... 26 7.4. Network Settings for Host Communications ........................................ 36 7.5. IO-Link Communication Status Check ................................................. 48 8. Initialization Method ................................................................................ 59 8.1. Initializing PLC ..................................................................................... 59 8.2. Initializing Slave Terminal .................................................................... ...

  • マニュアル

    ...Model CJ2M-CPU32 CJ1W-PA202 W4S1-05C CXONE-AL[][]C-V4 /AL[][]D-V4 (Included in CX-One) (Included in CX-One) - Version Ver.2.0 (Ver.2.12) Ver.1.00 Ver.4.[][] Ver.9.61 Ver.3.59c NX-EIC202 Ver.1.0 NX-ILM400 Ver.1.0 SYSMAC-NE001L Ver.1.16 (Included in Sysmac Studio) - Ver.2.2 E2E-X3B4-IL3 2M Ver.1.00 7 5.Applicable Devices and Device Configuration Precautions for Correct Use Update CX-Programmer and Network Configurator to the versions specified in this Clause 5.2. or to higher versions. If ...

  • マニュアル

    ...Normal/error detection processing. 4.2. Response code Sets the response code corresponding to the error in the setting response code storage area when an error occurs. Additional Information Refer to 9.8 Error Processing for information on the response codes. ...

  • マニュアル

    ...の見方 ...................................................................................56 S8BA-24D24D□□□LF 3 目次 4-4 動作モード設定.............................................................................................. 59 4-4-1 設定可能項目と説明 ......................................................................................................... 59 4-4-2 設定方法 ........................................................................................................................... ...

  • マニュアル

    ...24 23 22 21 20 19 18 17 48 47 46 45 44 43 42 41 40 39 38 37 36 35 34 33 62 61 60 59 58 57 56 55 54 53 52 51 50 49 ー ー BCD: Set the value as binary-coded decimal. Nodes to participate in the data links The value assigned indicates whether the node is to participate in the data links. Participate: 1 Not participate: 0 2-1 Controller Link Unit CJ1W-CLK21-V1 2-2. Usage Example of FB Component FB “Start Data Link” FB Name _CLK001_LINK_RunDatalink File Name _...

  • マニュアル

    ...-10CD/10C1D/20CD/20C1D/32CD CPM2□-S□ (*1) CPM2C-S100C/110C CPM2C-S110C-DRT CPM1/CPM1A (*1) CPM1(A)-10CDR/20CDR/30CDR/40CDR (-V1) CPM1A-10CDT/20CDT/30CDT/40CDT (-V1) CPM1A-10CDT1/20CDT1/30CDT1/40CDT1 (-V1) CQM1H CQM1H-CPU11/21/51/...

  • マニュアル

    ...10.7 AWG10 to 8 *1. For single-phase inputs, connect between any two phases out of the following: L1, L2, and L3. *2. The first value is for single-phase input power and the second value is for 3-phase input power. ...

  • マニュアル

    ...数 Hz 50/60 定格入力電流 Arms 8.4 16.0 23.0 40.0 定格出力電流 (FLA) Arms 11.3 14.5 22.6 33.9 61 三相 AC サーボモータ/ドライバ 1S シリーズ 取扱説明書  制御回路電源 • ドライバ容量が 3kW 以下定格 DC24V/1.2A 制御回路過電流保護が必要です。 • ドライバ容...

  • マニュアル

    ....0 70.0 85.0 105 135 160 195 230 290 2.5 4.0 5.5 9.2 14.8 19.0 25.0 32.0 39.0 48.0 61.0 75.0 91.0 112 150 180 217 260 VLD 40.0 37 3.1 316 110% 60sec / 120% 3sec LD 120% 60sec / 150% 3sec ND 150% 60sec / 200% 3sec 三相(3 線)380 ∼ 500V (受電電圧に依存します) VLD 2.8 3.7 5.8 8.7 12.1 17.3 21.5 27.7 32.6 43....

  • マニュアル

    ...Phone: +82-2-3218-5700 OMRON ELECTRONICS S.a.r.l AUSTRALIA Phone: 1-514-636-6676 Phone: +33-1-56-63-70-00 (French Language) OMRON ELECTRONICS ITALY PTY.LTD. UNITED KINGDOM OMRON ELECTRONICS S.r.l Phone: +...