全 916 件が検索されました。(481 - 500件を表示)

  • マニュアル

    ...CS1W-CN118 (See note.) PC-9801 BX PC-9801 BX NEC NEC CS1W-CN226 CS1W-CN626 Note 10-pin 9-pin female 9-pin female RS-232C port (9-pin female) XW2Z-200S-CV / 200S-V (2.0 m) XW2Z-500S-CV / 500S-V (5.0 m) XW2Z-200S-...

  • マニュアル

    ... number is changed). 174 Operating Procedures Section 11-2 Note The network type (i.e., Connects directly or Connects via network) should normally be set to Connects directly. Use the Connects via network setting when connecting the computer to a C-series or CVM1/...

  • マニュアル

    ... side of the instance. The value of the input source (data contained in the specified parameter just before the instance was called) will be passed to the input variable. P_On 1.0 FB EN ENO D0 D100 PV ...

  • マニュアル

    ...CS1W-CN118 (0.1 m) (See note 1.) CS1W-CN226 (2.0 m) CS1W-CN626 (6.0 m) CS1W-CN118 (See note 1.) CS1W-CN226 CS1W-CN626 9-pin 10-pin RS-232C port (9-pin female) XW2Z-200S-CV/200S-V (2.0 m) XW2Z-500S-CV/500S-V (5.0 m) XW2Z-200S-...

  • マニュアル

    ..., refer to the Product Guide in the package. For details on procedures for installing the CX-Drive from the CX-One FA Integrated Tool Package, refer to the CX-One Setup Manual (W463) provided with CX-One. Cat. No. W463 Model CXONE-@@@@...

  • マニュアル

    .../ALM INH PRPHL COMM CS/CJ-series PLC OPEN MCPWR L1 BUSY AC100-240V INPUT L2/N PERIPHERAL For Peripheral Port : CS1W-CN226 or CS1W-CN626 For RS-232C Port: XW2Z-200S-CV or XW2Z-500S-CV Or via network RUN OUTPUT AC240V DC24V PORT RS-422A/485 Modbus-RTU Inverter FREF FOUT IOUT MNTR F/R LO/RE PRGM RUN MIN MAX FREQUENCY STOP RESET SYSDRIVE DIGITAL OPERATOR PJVOP140 RUN ALARM *1. CS/CJ-series Serial Communications Board/Unit Ver. 1.2 or later. Required devices Model 3G3JV 3G3MV 3G3RV (-V1) Note Required Devices 3G3JV-PSI485J RS-422/...

  • マニュアル

    ... tables lists the Support Software that can be installed from CXOne and the reference manuals for each. Support Software Outline in CX-One CX-Programmer Application software to create and debug programs for SYSMAC CS/CJ/CP/NSJ-series, C-series, and CVM1/...

  • マニュアル

    ...DeviceNet networks. --- DeviceNet Manual CS1W-DRM21(-V1) CJ1W-DRM21 TM DeviceNet Unit Operation Manual Describes CX/CJ-series DeviceNet Units. C200HW-DRM21-V1 CVM1-DRM21-V1 TM DeviceNet Master Unit Operation Manual Describes C200H and ...

  • マニュアル

    ...procedures for a Controller Link Network. CS1W-CLK23, CS1W-CLK21-V1, Installation, setup, and operating procedures for the CJ1W-CLK23, CJ1W-CLK21-V1, Wired and Optical Controller Link Units. Controller Link C200HW-CLK21, CVM1-CLK21, Units are used to connect C200HX/HG/HE, ...

  • マニュアル

    ...or CX-Programmer Peripheral port CJ series Serial connection Either port can be used for connection. Host Link : Select SYSMAC WAY RS-232C Port Cables: Connection to Peripheral port: CS1W-CN226/626 Connection to RS-232C port: XW2Z-200S-...

  • マニュアル

    ...) Cyclic or extra tasks Steps, transitions, actions, jumps, subcharts Note: SFC elements are automatically registered to local variables. Series, divergence/convergence, simultaneous sequence divergence/convergence, jump Note: Number of divergences/convergences, simultaneous sequence divergences/convergences, and subcharts are unlimited. (Unlike with SFC for ...

  • マニュアル

    ... with an I/O Interface Unit. Programming Device Connecting Cable for peripheral (USB) port Commercially available USB cable USB 2.0 (or 1.1) cable (A connector - B connector), 5.0 m max. Programming Device Connecting Cables for serial port XW2Z-200S-...

  • マニュアル

    ...-3 Connection Method with a Serial Port Using a built-in RS-232C port makes it possible to connect Support Software with serial communications. Personal computer CX-One (e.g., CX-Programmer) D-Sub connector (9-pin, female) Recommended cable XW2Z-200S-...

  • マニュアル

    ...P_UF Greater Than or Equals Flag P_GE Not Equal Flag P_NE Less Than or Equals Flag P_LE Always ON Flag P_On Always OFF Flag P_Off Symbol Instructions Some of the C/CV-series PLC instructions have been changed to different instructions with the same functionality for the CP1E/CP2E-series PLCs. Instruction group CP1E/CP2E Series EQU AND= Data Movement MOVQ MOV Increment/Decrement INC ++B INCL ++BL Symbol Math Interrupt Control 2-4 C/...

  • マニュアル

    ... Value CV1 CV2 CV3 CV4 CV5 CV7 CV6 Output 0 Output 1 Soft Output 2 Soft Output 3 = Set in positive (+) direction = Reset in positive (+) direction = Set in negative (−) direction = Reset in negative (−) direction ...

  • マニュアル

    ... and mentainance procedures to take corrective actions for errors and conduct a routine inspection. Appendices This section provides the device profiles of Slaves that are required in the multi-vendor environments and gives a list of products including Multiple I/O Terminals and connected devices. CVM1/...

  • マニュアル

    ... to TRUE. When Sv_Ca_CountUp changes to TRUE, Sv_Cam_Disable is changed to FALSE. Retry processing for the MC_SaveCamTable instruction is completed. Sv_Ca_CTD Sv_Cam_Disable Sv_Ca_CountLoad INT#3 CTD Q CD Load ...

  • マニュアル

    ... with the CP2E CPU Unit. 4-4 Connection Method with a Serial Port Connection Method Connect the CX-Programmer to the serial communication port. Computer CX-Programmer D-Sub connector (9-pin, female) Recommended cable for CP1W-CIF01 XW2Z-200S-...

  • マニュアル

    ...1 2 3 4 5 6 V A Yrs °C s Branch output number 1 is lit. The "A" unit indicator will be lit when a current is displayed. The initial Setting Mode display is the abnormal current tripping threshold (CV) for branch output 1. The branch output that was most recently modified will be the current branch output regardless of the operating mode. Once the S8AS is switched to Setting Mode, it will not return to Run Mode automatically. (To return to Mode Selection Menu, press the neously for 3 seconds again.) and Keys simulta- For details on setting ...

  • マニュアル

    ...port on the CS/CJ-series PLC. This setting is required only when using the Host Link interface. • 1 or 2 bits IMPORTANT Always select the peripheral bus (ToolBus) interface when making a serial connection through the CS1W-CN226/626 or the XW2Z-200S-...