全 44 件が検索されました。(21 - 40件を表示)

  • マニュアル

    ...時間 M sp-7 比例帯 8.0 比例帯 M sp-6 M 40 M sp-5 水冷用比例帯 0.6 減少閾値 233 0 sp-4 M 8.0 M sp-3 水冷用比例帯 1.4 増大閾値 40 M sp-2 M d 目標値 1 水冷出力調整 off 機能 233 M sp-1 M i M PID 更新 off (適応制御) p M sp-0 a-ud w-dl M hs1 M...

  • マニュアル

    ... (Reference Point) is the fourth highest deviation of all the loops. 50 Sysmac Library User’s Manual for Temperature Control Library (W551) TempUniformityFilter The following figure shows the relationship between RefPointIndex (Reference Point Index) and RefPoint (Reference Point). Temperature SP[1] to ...

  • マニュアル

    ...0.00 to 99.59 14 Step 3 SP/Target SP 3 SP lower limit to SP upper limit 15 Ramp rate 3 16 Step 3 time/Soak time 3 0.00 to 99.59 17 Step 4 SP/Target SP 4 SP lower limit to SP upper limit 18 Ramp rate 4 19 Step 4 time/Soak time 4 0.00 to 99.59 20 Step 5 SP/Target SP 5 SP lower limit to SP upper limit 21 Ramp rate 5 22 Step 5 time/Soak time 5 0.00 to 99.59 23 Step 6 SP/Target ...

  • マニュアル

    ...0.00 to 99.59 14 Step 3 SP/Target SP 3 SP lower limit to SP upper limit 15 Ramp rate 3 16 Step 3 time/Soak time 3 0.00 to 99.59 17 Step 4 SP/Target SP 4 SP lower limit to SP upper limit 18 Ramp rate 4 19 Step 4 time/Soak time 4 0.00 to 99.59 20 Step 5 SP/Target SP 5 SP lower limit to SP upper limit 21 Ramp rate 5 22 Step 5 time/Soak time 5 0.00 to 99.59 23 Step 6 SP/Target ...

  • マニュアル

    ...0.00 to 99.59 14 Step 3 SP/Target SP 3 SP lower limit to SP upper limit 15 Ramp rate 3 16 Step 3 time/Soak time 3 0.00 to 99.59 17 Step 4 SP/Target SP 4 SP lower limit to SP upper limit 18 Ramp rate 4 19 Step 4 time/Soak time 4 0.00 to 99.59 20 Step 5 SP/Target SP 5 SP lower limit to SP upper limit 21 Ramp rate 5 22 Step 5 time/Soak time 5 0.00 to 99.59 23 Step 6 SP/Target ...

  • マニュアル

    ...0 NONE or STOP 1” NONE or RUN/STOP switching 1” NONE or 1 – (not disNONE or Multi–SP 2 set played) STOP points (set point 0/1 RUN/STOP switching switching) 2 – (not displayed) Multi–SP 4 set points (set point 0/1/2/3 switching) Note E5CN 11 12 EV1 EV2 13 4-5-2 “STOP (RUN/STOP) switching” can be set only on one of event input assignments 1 or 2. The event input on the side that is set can be used. The setting on the other side becomes “NONE”. When you are setting two external ...

  • マニュアル

    ... input 1 function NONE or STOP 1" NONE or RUN/STOP switching 1" Multi-SP 2 set points 1 - (not displayed) NONE or STOP (set point 0/1 switchĆ ing) 2 NONE or RUN/STOP switching Multi-SP 4 set points - (not displayed) *1 Event input 2 function (set point 0/1/2/3 switching) STOP (RUN/STOP) switching" can be set only on one of event input assignments 1 or 2. The event input on the side that is set can be used. The setting on the other side becomes NONE". • ( ' ( '/ " (& *" ' #$'#" )"' "$(' ("' & !#("' #" ' " ' -"(!% # !( '/ (&& & &' '# - #% - • " ' "(!% # !( '/ (&& & &' '# - 5-28 Event input 1 Selected Set ...

  • マニュアル

    ... 1” – (not displayed) 2 Event input 1 function Event input 2 function NONE or RUN/STOP switching 1” NONE or STOP Multi–SP 2 set points NONE or (set point 0/1 switch- RUN/STOP switching) ing Multi–SP 4 set points (set point 0/1/2/3 switching) – (not displayed) *1 “STOP (RUN/STOP) switching” can be set only on one of event input assignments 1 or 2. The event input on the side that is set can be used. The setting on the other side becomes “NONE”. E5AN 11 EV1 12 EV2 13 + EV1 + EV2 – When you ...

  • マニュアル

    ... and Main Functions Section 1-2 Control Adjustment • Optimum PID constants can be set easily by performing AT (auto-tuning) or ST (self-tuning). Event Inputs • With the E5CN-@@@B, the following functions can be executed using event inputs: switching set points (multi-...

  • マニュアル

    ...ON when an input error occurs. Control Adjustment • Optimum PID constants can be set easily by performing AT (auto-tuning) or ST (self-tuning). Event Inputs • With the E5@N-@@@B, the following functions can be executed using event inputs: switching set points (multi-...

  • マニュアル

    ... AT (auto-tuning) or ST (self-tuning). Event Inputs • With the E53-CN…B…N2 for the E5CN or the E5AN/EN-…M…-500-N with the E53-AKB for the E5AN/EN, the following functions can be executed using event inputs: switching set points (multi-...

  • マニュアル

    ... values, 4-6 reading CompoWay/F communications, 6-18 Modbus communications, 7-21 writing CompoWay/F communications, 6-21 Modbus communications, 7-23 writing in Protect Level CompoWay/F communications, 6-21 Modbus communications, 7-22 setting and changing the ...

  • マニュアル

    ...-15 Error Codes ..........................................................................................................................3-19 Section 4 V+ Process Manager Module 4-1 pm.ace.blt.cam .......................................................................................................................4-3 4-2 pm.ace.blt.ltch........................................................................................................................4-4 4-3 pm.ace.blt.pos........................................................................................................................4-5 4-4 pm.ace.blt....

  • マニュアル

    ...-14,5-12 システム構成・・・・・・・・・・・・・・・・・・・・・・・・・・ 1-2 システムアラーム・・・・・・・・・・・・・・・・・・・・・・ 7-4 システムアラーム情報・・・・・・・・・・・・・・ 4-9,7-5 終端抵抗・・・・・・・・・・・・・・・・・・・・・・・・・・・・・・ 3-3 主設定値(SP)・・・・・・・・・・・・・・・・・・・・ 4...

  • マニュアル

    ...量の制限 …………………………………… 4-5 目標値リミッタ ………………………………… 4-6 SPランプ ………………………………………… 4-6 4.3 イベント入力の使い方 …………………………… 4-8 入力の割付 ……………………………………… 4-8 マルチSP ………………………………………… 4-9 他のイベント入力機能 ………………………… 4-10 4.4 リモートSPの使い方 ……………………………… 4-11 スケーリング …………………………………… 4-11 SPモード ………………………………………… 4-11 リモートSPモニタ ……………………………… 4-12 SPトラ...

  • マニュアル

    ...量の制限 …………………………………… 4-5 目標値リミッタ ………………………………… 4-6 SPランプ ………………………………………… 4-6 4.3 イベント入力の使い方 …………………………… 4-8 入力の割付 ……………………………………… 4-8 マルチSP ………………………………………… 4-9 他のイベント入力機能 ………………………… 4-10 4.4 リモートSPの使い方 ……………………………… 4-11 スケーリング …………………………………… 4-11 SPモード ………………………………………… 4-11 リモートSPモニタ ……………………………… 4-12 SPトラ...

  • マニュアル

    ...演算結果 ------------- 割付例 -------------------------4.4 混合演算 ---------------------------4.5 PIDの切替 ------------------------- PID組について -------------- PID自動選択 -----------------4.6 SP設定の応用 -------------------- SP変化率リミッタ ---------- リモート...

  • マニュアル

    ...ニュアル操作 ‥‥‥‥‥‥‥‥‥‥ 3-12 マニュアル操作量 ‥‥‥‥‥‥‥‥‥ 5-5 マニュアルモード ‥‥‥‥‥‥‥ 1-6、 5-5 マニュアルリセット値 ‥‥‥‥‥‥‥ 5-13 マルチSP ‥‥‥‥‥‥‥‥‥‥‥‥‥ 4-8 ∼使用数 ‥‥‥‥‥‥‥‥‥‥‥‥ 5-33 む A/Dコンバータ異常 ‥‥‥‥‥ 3-5、 5-25、 7-5 ASCIIコード表 ‥‥‥‥‥‥‥‥‥‥ A-14 AT ‥‥‥‥‥‥‥‥‥‥‥‥‥‥ 1-3、 3-13 ∼算出ゲイン ‥‥‥‥‥‥‥‥‥‥ 5-30 ∼実行/中止 ‥‥‥‥‥‥‥‥‥‥ 5-10 ∼ヒステリシス ‥‥‥‥‥‥‥‥‥ ...

  • マニュアル

    ...ラン/ストップの切り替え※ 1 マルチ SP 2 点なしまたはラ ン / ス (目標値 0/1 の切 トップの切り替えり替え) マルチ SP 4 点 (目標値 0/1/2/3 の切り替え) −(非表示) 2 ※ 1 「STOP(ラン/ストップの切り替え)」はイベント入力割付1または 2の片方のみ設定...

  • マニュアル

    ...ラン/ストップの切り替え※ 1 マルチ SP 2 点なしまたはラ ン / ス (目標値 0/1 の切 トップの切り替えり替え) マルチ SP 4 点 (目標値 0/1/2/3 の切り替え) −(非表示) 2 イベント入力 2 の機能 ※ 1 「STOP(ラン/ストップの切り替え) 」はイベント入力割付1ま...