全 27 件が検索されました。(21 - 27件を表示)

  • マニュアル

    .... • Residual voltage with transistor turned on: 3 V max. • Current leakage with transistor turned off: 1.5 mA max. • Switching load current: 20 mA or greater. Approximately 5 V is imposed between COM and terminals 5 to 7 with a current flow of approximately 18 ...

  • マニュアル

    .... • Residual voltage with transistor turned on: 3 V max. • Current leakage with transistor turned off: 1.5 mA max. • Switching load current: 20 mA or greater. Approximately 5 V is imposed between COM and terminals 5 to 7 with a current flow of approximately 18 ...

  • マニュアル

    ...Connection Terminal X Axis 10 11 Y Axis 32 33 X Axis 9 11 Y Axis 31 33 Specification Input current is 6 mA (at 12 V)) to (at 24 V); o 13 3 mA (a ); f other specifications remain the same Signal is a line-driver ssignal g a corresponding co espo d g to o S Am26LS31 Response Time Mode 0: < 1 ms s Mode 1, 2: <0 0.1 1 ms Mode 3: Not used Output Specifications Item 242 Specification Maximum switching capacity Minimum switching capacity Leakage current 30 mA at 5 to 24 VDC ±10%\(NPN ...

  • マニュアル

    ... by the sensor is 10 centimeters and the output of the sensor is 15 mA when the length of the object is 30 centimeters, the following data should be input. X1 = 400, X2 = 1500, Y1 = 1000, Y2 = 3000 If the input from the sensor is 10 ...

  • マニュアル

    .... 96 Section 6-2 Specifications and Part Names Line Disconnection Detection (Analog Inputs) If the input signal drops to below 0.8 V or 3.2 mA, respectively, when the input range is set to either 1 to 5 V or 4 to 20 ...

  • マニュアル

    ... mA The current range 4 to 20 mA corresponds to 0000 to 1770 hex (0 to 6,000). The convertible data range is FED4 to 189C hex (–300 to 6,300). If the input current is below the input range (input current less than 3.04 ...

  • マニュアル

    ... which conversion is possible is 3.2 to 20.8 mA and here the output data is FED4 to 189C Hex (–300 to +6300). If the input value falls below the input range such as for a disconnected line (input current is less than 3.04 ...