全 24 件が検索されました。(21 - 24件を表示)

  • マニュアル

    ...いて次のような場所には設置しないでください。 ・周囲温度が 0 ∼ +50℃の範囲を超える (ただし、ビデオモニタ推奨品 形F150-M09-2Dの周囲温度は、0∼+40℃) ・温度変化が急激で結露する・相対湿度が 35 ∼ 85%RH の範囲を超える・腐食性ガス、可燃性ガスがある・塵...

  • マニュアル

    ..., connect it to the video input connector using a BNC-RCA connector in the way shown below. Video input connector (BNC type) BNC-RCA connector (See note.) RCA plug Note 3-36 A BNC-RCA connector is provided with the Monitor Cable (...

  • マニュアル

    ...The V530-R150 is highly reliable and resistant to most environmental factors. The following guidelines, however, must be followed to ensure reliability and optimum use of the V530-R150. Components Be sure to use the Camera, Camera Cable, and Console designed for the V530-R150. • Camera (...

  • マニュアル

    ... environmental factors. The following guidelines, however, must be followed to ensure reliability and optimum use of the V530-C300E. Components Be sure to use the Scanner, Scanner Cable, and Console designed for the V530-C300E. • V530-H30@ Scanner • V530-W001 Scanner Cable • ...