全 344 件が検索されました。(301 - 320件を表示)
- マニュアル
...ED ST Data CR+LF 256 bytes max. 256 bytes max. • Only the first start code is valid if there is more than one start code. • Only the first end code is valid if there is more than one end code. • Use CF...
- マニュアル
..., the rack number is 0 and the slot number is 3 (unit number 1). EM/EXT Replace? ?-?= … 0 Replace? 0-?= … ✽EM Specify rack number 0. 3 Replace? 0-3= … Specify slot number 3. CF SRCH Replace? 0-3=NS01 … The Unit type is displayed. ...
- マニュアル
...Model S3200-COCF2011 S3200-COCF2511 Replacement model S3200-COCF2071 S3200-COCF2571 Optical Fiber Cables with Connectors (Indoor Use Only) The following Optical Fiber Cables are available with Connectors (lap/polished type) already attached. Note Specifications Optical Fiber Cable Connectors: ...
- マニュアル
... 127 PART 2: CX-Server PLC Tools OMRON APPENDIX B – PLC Memory Areas Prefix Start Channel End Channel Word Addressing Bit Addressing Read Write D 0 32767 Yes No Yes CF 0 11 No Yes No CF 100 104 No Yes No ...
- マニュアル
... 127 PART 2: CX-Server PLC Tools OMRON APPENDIX B – PLC Memory Areas Prefix Start Channel End Channel Word Addressing Bit Addressing Read Write D 0 32767 Yes No Yes CF 0 11 No Yes No CF 100 104 No Yes No ...
- マニュアル
... 129 PART 2: CX-Server PLC Tools OMRON APPENDIX B – PLC Memory Areas Prefix Start Channel End Channel Word Addressing Bit Addressing Read Write D 0 32767 Yes No Yes CF 0 11 No Yes No CF 100 104 No Yes No ...
- マニュアル
...-6 CFast Card Slot (Optional) Depending on the product configuration an optional CFast Card slot is located at the rear side of the base layer. The CFast Card slot accepts CFast Cards that comply with the CFast 2.0 specification. 3 t as ...
- マニュアル
... was received. 2A Group 2 only server general failure This error code is reported only by group 2 only servers with 4K or less of code space and only in place of Service not supported, Attribute not supported, or Attribute not settable. 2B-...
- マニュアル
...4-4-13 Controller Control Command (CC) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-14 Error Information Read Command (CF) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-15 Test Command (TS) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-16 Abort Command (XZ) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-17 Command Undefined Response (IC) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-18 Error Response . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 4-4-19 End Code List . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Example of Communications Program . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 24 28 28 28 29 32 36 36 37 37 38 39 40 40 41 42 42 43 44 45 45 46 46 46 47 47 48 23 Section Movement of Data Carrier and Command Status 4-1 4-1 Movement of Data Carrier and Command Status Communications Control Procedure The ...
- マニュアル
...Z500-SW2T Aperture Label PEAK POWER 15000 µw PULSE DURATION 25000 µs WAVE LENGTH 658 AVOID EXPOSURE Laser radiation is emitted from this aperture O Th M Sh R 21 is Pla Kyo iokoON CF las to ji C R er M AYAce o 600 Hori orp 10 pr an B f -8 ka o 4 od ufa E F ma 530 wa rati 0.1 uc ctu acto nu JA , Sh on 0 a t co nd m re ry, fac PAN imo d OM tu gy 10 plie in R re o-k 40 s O : u, N ....
- マニュアル
... of a variable within the variable area using the variable type and address. Variable types in variable areas are as follows: Variable type C4 C5 C6 C7 C8 C9 CA CB CC CD CE CF D0 D1 D2 D3 ● Addresses (Communication/ CompoWay/F) Description Communication monitor Protect level RUN level Adjustment level Adjustment level 2 Bank setting level PID setting level Approximation setting level Input initial setting level Control initial setting level Control initial setting 2 level Alarm setting level Display adjustment level Communications setting level Special function setting level Expansion control setting level Area Setting area 0 (during ...
- マニュアル
... to I5 (6 bits) Q0 to Q7 (8 bits) Q0 to Q3 (4 bits) Timers T0 to Tf (16 bits) T0 to T7 (8 bits) Holding timers #0 to #7 (8 bits) #0 to #3 (4 bits) Counters C0 to Cf (16 bits) C0 to C7 (8 bits) Weekly timers @0 to @f (16 bits) @0 to @f7(8 bits) Calendar timers 0 to Displays 7-1 ZEN-10C@@@-@ I0 to Ib (12 bits) f (16 bits) 0 to D0 to Df (16 bits) Work bits M0 to Mf (16 bits) Holding bits H0 to Hf (16 bits) Expansion ...
- マニュアル
...[Z204-E1-02] V670-CF01/D13F01(H)/D13F03 Electromagnetic Inductive RFID System User's Manual Electromagnetic Inductive RFID System V670 Series User's Manual CF Reader/Writer V670-CF01 ID Tag V670-D13F03 V670-D13F01 V670-D13F01H Cat. No. Z204-E1-02 Standard Conformity (Be sure to read.) SECTION 1 Product Outline SECTION 2 Communications Preparations SECTION 3 Functions SECTION 4 Commands SECTION 5 Troubleshooting SECTION 5 SECTION 6 Appendices (Specifications and Dimensions, Characteristics Data Based on Operating Conditions, Memory Map, Maintenance and Inspection, Table of JIS8 Unit Code (ASCII), Degree of Protection) SECTION 6 SECTION ÇÕǹÇ?Ç...
- マニュアル
...RUN RUN ZFV ZS-DSU User’s Manual 1-11 Section 1 Part Names and Functions Part Names and Functions Section 1 FEATURES The following describes the names and functions of parts on the Data Storage Unit. (1) ...
- マニュアル
...T0 to Tf (16 timers) # Holding timers #0 to #7 (8 timers) @ Weekly timers @0 to @f (16 timers) (See note 1.) * Calendar timers *0 to *f (16 timers) (See note 1.) C Counters C0 to Cf (16 counters) F 8-Digit counter F0 (1 counter) A Analog comparators A0 to A3 (4 comparators) (See note 2.) P Comparators P0 to Pf (16 comparators) G 8-Digit comparators G0 to G3 (4 comparators) Note 64 Bit type and number CPU Unit input bits 1. Can be used only when LCD-type CPU Units are used. 2. Can be used only ...
- マニュアル
...0000 to 0F00 Holding timer PV #0 to #7 (8 timers) Weekly timer operation mode @0 to @f (16 timers) Weekly timer SV Calendar timer SV *0 to *f (16 timers) C6 0000 to 0F00 Counter PV C0 to Cf (16 counters) C0 0006 to 0F06 C3 0000 to 0F00 Counter SV ● Reading Comparators RS-485 communications can be used to read the variable area and perform comparisons with the following three types of comparators. 1. Analog Comparators: Compare an analog input with a constant or two analog inputs. 2. Comparators: Compare the present value of a timer, holding timer,...
- マニュアル
... type and number T Timers T0 to Tf (16 timers) # Holding timers #0 to #7 (8 timers) @ Weekly timers @0 to @f (16 timers) * Calendar timers *0 to *f (16 timers) C Counters C0 to Cf (16 counters) F 8-Digit counter F0 (1 counter) A Analog comparators A0 to A3 (4 comparators) (See note.) P Comparators P0 to Pf (16 comparators) G 8-Digit comparators G0 to G3 (4 comparators) Note Can be used only with CPU Units with DC power supplies (PNP connection). ▼ Press the ALT Button to enable drawing a connection line. The left arrow cursor ...
- マニュアル
...Name More information Description TS TEST Used to check communications between the ID Controller and the host device. Returns the test message sent from the host device without any changes. CC CONTROLLER CONTROL Used to manipulate user I/O. ...
- マニュアル
...Check if the system starts with the camera cable disconnected. Data corruption: ● The scene group data and system data saved to the controller have been corrupted. In some cases when the power is shut down or the USB memory was removed while accessing the ...
- マニュアル
... Format The output CSV file format can be changed according to the external device. Item Symbol Field separator None, comma (default), tab, space, or semicolon Decimal symbol None, point (default), or comma Record separator None, comma, tab, space, or CR or ...