全 307 件が検索されました。(261 - 280件を表示)

  • マニュアル

    ...24VDC DataSettingCensole C200H-DSCOI " 蹴鯨 LoOP1 Temperature sensor Extruder Heater Valve L◎◎P2 Temperature sensor C◎olant Current Tra「lsformer CT) Heatθr Valve Remotel!◎「Fe「minalo「 ConnectorTerminat ...

  • マニュアル

    ... connector. The individual shields must be electrically insulated from the external shield. Individual signal shields Signal wires Insulation Individual signal shields External shield Cover Cover B: R: G: W: O: Y: Gr: ...

  • マニュアル

    ...CQM1-MP08R Clock Function No Yes No Yes No Yes Memory 4K-word EEPROM 8K-word EEPROM EPROM IC socket only. y EPROM chip p not included. Refer to the following g table bl ffor d details il on available il ...

  • マニュアル

    .../itConfig{ノrationsfordetails, 17 ---------------------[End of Page 2734]--------------------- 1/OCircuitConf》gurations Section3四3 3・3 3・3・1 1/OCircuitc◎nfigurati◎ns Enc◎dergnputCircuitC◎nfiguration Circuit 多多多タ多多 pin BO AO ...

  • マニュアル

    ...WhenblockNOO8containsthepassmodefundion(GIO),blocksNOlland NO12arepre・executedwhileNOlOisbeingexecuted,soblockNO12won'tbe skippedifoptionalinput3isturnedONafterexecutionofblockNOIO. ToensurethatblockNO12willbeskipped,makesurethatopt泊nalinput3isON beforeblockNO10isexecuted. Speed Optional input3 BbckNO12isn'tskdppedbecause optionalinput3isn'tONwhenb│ock NOIIispre-executed. ■me Speed 1 Optional i叩ut3 1nthiscase,...

  • マニュアル

    ... in bits 8 to 15 of address 14 in RAM) RAM). If the scaling function is disabled, disabled conversion data is taken immediately before D/A conversion. If the scaling g f i is i enabled, bl d conversion i function data is in engineering units. (This data is scaled and then subject to D/A conversion.) 0 to 15 7 1 2 3 4 5 6 7 8 1 2 3 4 5 6 7 8 Description Output p Ramp p E ...

  • マニュアル

    ...With cable (2 m) C200H-PRO27-E C200H Programming Console Hand-held, with backlight; requires the C200H-CN222 or C200H-CN422, see below. C200H-CN222 C200H-CN422 C200H-ATT01 WS02-CXPC1-E C200H-PRO27-E Connecting g C ...

  • マニュアル

    ...ERROR Commanderror 5 CONNECT1200 Connectionto1,200bp8 6 NODIALTONE No白diaトtonedetection 7 BUSY Busydetection 8 NOANSWER Noanswe『detection 9 HANDSETINUSE Busy 234 CONNECT2400ゾREL4 Connectionto2400MNPclaSS Dlsasser論...

  • マニュアル

    ... FG terminal on the Rack. 12 Section LED Indicators 2-2 2-2 LED Indicators The following table shows the meaning of the LED indicators. Indicator FAIL Name SYSFAIL Color Red PASS SYSFAIL di bl d disabled Green COMM (NS) Network status Green Red Status ON OFF ON OFF ON Flashing ON Flashing HEALTH (MS) Module status --- OFF Green Red ON ON --- OFF Meaning A SYSFAIL occurred. A SYSFAIL hasn’t occurred or the SYSFAIL signal is disabled. The SYSFAIL signal is disabled. The SYSFAIL signal is enabled. Communications established (Normal network status) Communications not yet established (The network ...

  • マニュアル

    ...Terminating Continuous Automatic Bank end Start Terminating Continuous Automatic Bank end Deceleration stop Input CW/CCW limit. INDEPENDENT START from OFF to ON when h Sequence S Number N b Enable E bl...

  • マニュアル

    .... . . . . . . . . . 5-20-1 Binary Addition: +(400)/+L(401)/+C(402)/+CL(403) . . . . . . . . . . . . . . . . . . . . . 5-20-2 BCD Addition: +B(404)/ +BL(405)/+BC(406)/+BCL(407) . . . . . . . . . . . . . . . . . 5-20-3 Binary Subtraction: –(410)/ –L(411)/–C(412)/–CL(413) . . . . . . . . . . . . . . . . . . . 5-20-4 BCD Subtraction: –B(414)/ –...

  • マニュアル

    ... 32 input points and 32 output points. Model number CPM1A-DRT21 Appendix A Standard Models Adapters and Connecting Cables (1:1 Connection) CPM2A port Peripheral RS-232C Name RS-232C Adapter Appearance RS-232C C ...

  • マニュアル

    ...When the block diagram is selected When a step ladder program is selected When a sequence table is selected Overview of User Interface Menu Settings, g , i d continued Submenu/ Command Function Cut Bl k Block Copy Paste Increment Block Address FBD Copy Paste User-defined Blocks Section Description Cuts a function block from the Project Workspace. Copies a function block in the Project Workspace. Pastes a function block in the Project Workspace. Selects and increments the function block address by 1. If the next address is being used, it is also incremented by 1. 2-2 Conditions for selection...

  • マニュアル

    ... code 1st byte (Hex) Correction 2nd byte (Hex) Recorded in EEPROM Command block Bits 0 to 7: Source node address Bits 8 to 14: Source Network address Bit 15: OFF Check routing tables. R bl k Response block Bits 0 to 7: Destination node address Bits 8 to 14: Destination Network address Bit 15: ON Check routing tables and system configuration. Do not try to access Networks separated by more than one other Network. No Be sure to use the correct FINS command format. No (1st byte: bits 8 to 15 15; 2nd byte, bits 0 to 7) 9-...

  • マニュアル

    ...OK OK INCREMENT BCD ++B/ @++B 594 Increments the 4-digit BCD content of the specified word by 1. OK OK OK OK OK OK OK OK DOUBLE INCREMENT BCD ++BL/@++ BL 595 Increments the 8-digit BCD content of the specified words by 1. OK OK OK OK OK OK OK OK DECREMENT BCD --B/ @--B 596 Decrements the 4-digit BCD content of the specified word by 1. OK OK OK OK OK OK OK OK DOUBLE DECREMENT BCD --...

  • マニュアル

    ...++L @++L 591 ++L Wd DECREMENT BINARY -@-- 592 -Wd DOUBLE DECREMENT BINARY --L @--L 593 --L Wd INCREMENT BCD ++B @++B 594 ++B Wd DOUBLE INCREMENT BCD ++BL @++BL 595 ++BL Wd DECREMENT BCD --B @--B 596 --B Wd DOUBLE DECREMENT BCD --...

  • マニュアル

    ... UPS Communication Cable Communication cable details are provided below. OMRON is not responsible for the operation or performance of any other brand of communication cable. Model S8BW-C02 3-34 Appearance Cable length 2m Specifications Signals for • Signal output (...

  • マニュアル

    ...2-10-10 UPS Communication Cable Communication cable details are provided below. OMRON is not responsible for the operation or performance of any other brand of communication cable. Model S8BW-C02 Appearance Cable length 2m Specifications Signals for • Signal output (...

  • マニュアル

    ... State Contactor for Three-phase Motor Control Harmonized protection is ensured for motor overcurrents. Be sure to supply power to the G3J through a fuse or non-fuse breaker to protect the G3J from damage due to short-circuiting. Standard Models DC-input Models G3J-@...

  • マニュアル

    ... Video Monitor screen during measurement. “RAW” means raw image, “BIN” means binary-coded image, and “MIX” means a compound of raw and binary-coded images. B/W Shows that a black or white image is selected for the object to be measured. “...