全 235 件が検索されました。(201 - 220件を表示)
- マニュアル
... bit or word to see where and how the bit or word is being used. Used during program changes and debugging. C-series PC Any of the following PCs: C2000H, C1000H, C500, C200H, C40H, C28H, C20H, C60K, C60P, C40K, C40P, C28K, C28P, C20K, C20P, ...
- マニュアル
..., and other Units. The CPU Rack, along with the Expansion CPU Rack, provides both an I/O bus and a CPU bus. C-series PC Any of the following PCs: C2000H, C1000H, C500, C200H, C40H, C28H, C20H, C60K, C60P, C40K, C40P, C28K, C28P, C20K, C20P, ...
- マニュアル
..., and other Units. The CPU Rack, along with the Expansion CPU Rack, provides both an I/O bus and a CPU bus. C-series PC Any of the following PCs: C2000H, C1000H, C500, C200H, C40H, C28H, C20H, C60K, C60P, C40K, C40P, C28K, C28P, C20K, C20P, ...
- マニュアル
... mode), display terminal, printer, display BSC31/BSC41 BSC51/BSC61 Computer (with terminal mode), display terminal, printer, display Computer (with terminal mode), display terminal, printer, display NA Host Link Unit (C500-LK203, NA C500-LK201-V1, C200H-LK202, and ...
- マニュアル
..., and other Units. The CPU Rack, along with the Expansion CPU Rack, provides both an I/O bus and a CPU bus. C-series PC Any of the following PCs: C2000H, C1000H, C500, C200H, C40H, C28H, C20H, C60K, C60P, C40K, C40P, C28K, C28P, C20K, C20P, ...
- マニュアル
... number APF/PCF C200H-LK101-PV1 RS-422 C200H-LK202-V1 RS-232C C200H-LK201-V1 C1000H/C2000H PCF 3G2A6-LK101-EV1 C500 APF/PCF 3G2A6-LK101-PEV1 C200H RS-232C 3G2A6-LK201-EV1 C120 RS-422 3G2A6-LK202-EV1 PC Link Unit Single level: 32 Units Multilevel: 16 Units RS-485 C200H-LK401 Remote I/O M Master U i Units Up to two per PC; connectable to up to 5 Sl Slaves per PC totall Remote I/O Slave Units 100 to 120/200 to 240 VAC (switchable) APF/PCF Wired APF/PCF C200H-RM001-PV1 C200H-...
- マニュアル
...-LK202-V1 RS-232C C200H-LK201-V1 C1000H/C2000H PCF 3G2A6-LK101-EV1 C500 APF/PCF 3G2A6-LK101-PEV1 Appendix A Standard Models Name Specifications Model number C200H RS-232C 3G2A6-LK201-EV1 C120 RS-422 3G2A6-LK202-EV1 PC Link Unit Single level: 32 Units Multilevel: 16 Units RS-485 C200H-LK401 Remote I/O M Master U i Units Up to two per PC; connectable to up to 5 Sl Slaves per PC totall Remote I/O Slave Units 100 to 120/200 to 240 VAC (switchable) APF/PCF Wired APF/PCF C200H-RM001-PV1 C200H-RM201...
- マニュアル
... slots next to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the ...
- マニュアル
...x 161 x 160 x 161 x 160 End code Model code FCS ↵ Terminator Model Code “Model code” indicates the PC model in two digits hexadecimal. Model code Model 01 C250 02 03 C500 C120 0E 10 C2000 C1000H 11 12 C2000H/CQM1/CPM1/CPM1A/SRM1 C20H/C28H/C40H/C200H/C200HS 20 21 CV500 CV1000 22 40 CV2000 CVM1-CPU01-E 41 42 CVM1-CPU11-E CVM1-CPU21-E 6-3-29 TEST–– TS Returns, unaltered, one block of data transmitted from the host computer. Command Format @ x 101 x 100 Node no. Response Format x 101 x 100 Node ...
- マニュアル
...Model code FCS ↵ Terminator 425 Host Link Commands Parameters Section 11-3 Model Code “Model code” indicates the PC model in two digits hexadecimal. Model code Model 01 C250 02 C500 03 C120 0E C2000 10 C1000H 11 C2000H/CQM1 12 C20H/C28H/C40H/C200H/C200HS 20 CV500 21 CV1000 22 CV2000 40 CVM1-CPU01-E 41 CVM1-CPU11-E 11-3-29 TEST–– TS Returns, unaltered, one block of data transmitted from the host computer. Command Format @ x 101 x 100 Node no. T : 122 characters max. S Header code FCS Characters ↵ Terminator Response Format @ x 101 x 100...
- マニュアル
...-CN425 Connecting Cable Used to connect an IBM PC/AT or compatible to the C200HS. 3.3 m CQM1-CIF02 Ladder Support Software (LSS) Name Specifications Ladder Support Software (for C20, CjjP,, CjjK, C 0, Cjj Cjj , ...
- マニュアル
... from SR word (0300) whether a communications error has occurred. For details, refer to the SYSMAC C Series Remote I/O Unit (Wired Type) Operation Manual for details. 132 Section 5-5 Troubleshooting Communications Errors 5-4-1 RM Unit SR Area ...
- マニュアル
... next to the CPU free. It is not possible to use devices connected to the CPU (such as the Programming Console) if these slots are occupied. If the C200H Slave Rack is connected to another SYSMAC model Remote I/O Master Unit, such as the ...
- マニュアル
... mm PFP-100N2 End Plate --- PFP-M Spacer --- PFP-S Standards --- Note: Order DIN Tracks, End Plates, and Spacers in units of 10 each. SYSMAC-CPT Support Software Name SYSMAC Support Software (for C20, CjjP, CjjK, ...
- マニュアル
...thesameprogramoraseparateprogram.CopyingleavestheoriginaI datainplaceandplacesthecopieddataintheWindowsclipboard. counter C】PU CrossReferenceTable C-SeriesPLC AfUnctionusedtocountthenumberoftimesabitorexecution conditionhaschangedfromOFFtoONorviceversa. StandsforCentralProcessingUnit,themicroprocessingchipthat controlsaPLC. OneofthefburavailableTableviewsinSYSMAC-CPT.TheCross Referencetableviewdisplaysallreferencestoeveryaddressusedina PLCprogram. AnyofthefollowingPLCs:C2000H,ClOOOH,C500,C200,C200H, C200HE,C200HE-Z,C200HG,C200HS,C200HX,C200HX-Z, C2eOHZ,...
- マニュアル
... those slots, it will not be possible to mount tools such as the Programming Console. • Special I/O Units cannot be used with C200H Remote I/O Slave Racks that are connected to Remote I/O Master Racks for other SYSMAC Programmable Controller models (such as ...
- マニュアル
... with the Expansion CPU Rack, provides both an I/O bus and a CPU bus. crystal optical fiber cable See AGF. C-series PC Any of the following PCs: C2000H, C1000H, C500, C200H, C40H, C28H, C20H, C60K, C60P, C40K, C40P, C28K, C28P, C20K, C20P, ...
- マニュアル
..., and other Units. The CPU Rack, along with the Expansion CPU Rack, provides both an I/O bus and a CPU bus. C-series PLC Any of the following PLCs: C2000H, C1000H, C500, C200H, C40H, C28H, C20H, C60K, C60P, C40K, C40P, C28K, C28P, C20K, C20P, ...
- マニュアル
... PLC: CS1G, CS1G-H, CS1H, CS1H-H, CJ1G, CJ1G-H, CJ1H-H, CJ1M. C-Series Indicates any one of the following types of PLC: C2000H, C200H, C200HE, C200HE-Z, C200HG, C200HE-Z, C200HS, C200HX, C200HX-Z, C1000H, C**H, C**K, C**P, CQM1, C500, ...
- マニュアル
... 9 as the 4th digit of the lot number. (The lot number may be 4 or 5 digits long.) Note 2: Only host link mode can be used. 26 USB to PLC/PT Connection Tables ● C-series Host Link Unit (C200H-LK201-V1 or ...